Part Number: LM5001-Q1 Other Parts Discussed in Thread: LMT84 Dear all,
I want to add thermistor to change Vout depending on ambient temperature for organic light emitting display (OLED).
Is this way recommended? Have you tested like this way?
* I will…
Part Number: LM5001 Hello guys,
One of my customers is considering using LM5001 for their new products. They want to design a variable output voltage power supply (PS) using LM5001. Their target PS spec is the follow. Vin=5V, Vout=6V~40V, Io=50mA, variable…
Other Parts Discussed in Thread: LM5001-Q1 Dear Support Team
How much is the LM5001-Q1 startup voltage when It is used in SEPIC?
If LM5001-Q1 can not operate at around 3.1V in start up, Could you teach the device which can work around 3V of start up in the following…
Other Parts Discussed in Thread: LM5001-Q1 Hi,
My customer has question about LM5001-Q1. Could you tell me about questoin?
[Question] Is there any sequence requirement between EN and external synchronization clock of RT? My customer considers to input external…
Frederic,
Would you re-post your question into the non-isolated DC-DC forums? They should be able to help you with the model there.
e2e.ti.com/.../
Thanks,
-Clancy
Dear all,
Could you teach me about minimum voltage of 'VIN to GND'?
I saw term 6.1 of data sheet, but data sheet only mentioned maximum voltage.
Best regards,
Other Parts Discussed in Thread: LM5001-Q1 , TINA-TI Dear all,
About LM5001-Q1,
I would like to know the amount of current flowing along VIN pin.
At the page.11 of data sheet '8.1.1 VIN', you say that the current into the VIN pin depends on different…
Other Parts Discussed in Thread: LM5001-Q1 Dear all,
I compare LM5001-Q1's datasheet page.17 with PMP9481 schematic.
I would like to know the difference LM5001-Q1's datasheet and PMP9481.
Relative to LM5001-Q1's datasheet, PMP9481 schematic has…
Dear all,
I would like to know about internal shunt resister behavior when SW FET is breakdown.
If SW FET is breakdown, will internal shunt resister be open break?
Best regards,