Part Number: LM5006 Other Parts Discussed in Thread: LM5161 , LM5166 Hello,
When using a LM5006 to supply a 5V rail from a 15-70V source, I encountered an unexpected behavior concerning the shutdown/start-up sequence. If the LM5006 is started after a…
Other Parts Discussed in Thread: LM5160 , LM5006 I would like to use LM 5006 and derive two DC outputs ( i.e 19 V DC to deliver 1.5 A and 12 V DC to deliver 1 A) from 48 V DC. Any solutions ?
Other Parts Discussed in Thread: LM5006 I'm currently using the LM5006 and recently took it in for EMI testing and found that there was a lot of noise around 185MHz. Upon closer investigation, there is ringing at 185MHz at every switching cycle. I…
Other Parts Discussed in Thread: LM5006 I'm currently using the LM5006 and recently took it in for EMI testing and found that there was a lot of noise around 185MHz. Upon closer investigation, there is ringing at 185MHz at every switching cycle. I…
Other Parts Discussed in Thread: LM5006 I am using the LM5006 in a very, very space constrained application. The datasheet shows two input capacitors - C1 and C5. C5's state purpose is to "help avoid supply voltage transients and ringing due to long lead…
Other Parts Discussed in Thread: LM5006 I see on the LM5006 eval board, Vout is set to 5V, and the output capacitor (C2) is 15uF, 16V, X7R. I have used this exact part in my design and it is working well. However, I am hoping to replace this capacitor…
Other Parts Discussed in Thread: LM5010A , LM5006 The LM5006 and LM5010A look like very similar parts, with very similar application circuits (especially when using a diode for the LM5006 instead of a FET).
I am currently using the LM5006, and do not need…
Other Parts Discussed in Thread: LM5006 I am using the LM5006 with the flyback diode to allow the regulator to take advantage of DCM when there is no load.
On one of my boards, every so often the SW ON pulse lasts longer than normal, allowing Vout to spike…
Other Parts Discussed in Thread: LM5006 , LM5007 , LM25007 Hello,
I am using the LM5006 regulator. I am getting good performance, but I would like to try to lower the current drawn by the system when there is no load and the regulator is enabled and switching…
Other Parts Discussed in Thread: LM5006 I am using the LM5006, and I need to add a delay of ~10 seconds from when input voltage is applied until the regulator generates an output (5V in my case).
Timing accuracy is not very important. +/- 50% should be…