Part Number: LM5010A Hello. The pin layout is extremely inconvenient in the 14-pin package, and I would like to use unused pins as duplicates. DS says that i can connect NC pins to ground plane to improve heat dissipation. But can i connect NC pins to…
Part Number: LM5010A-Q1 Hi Team, We have a customer that go through this article:
The customer would like to ask the following regarding the article above:
- Can this method also be applied to the LM5010A-Q? - Is this method only suitable for small voltage…
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010 Hello,
I am after LM5010A-Q0, which is the same part but has higher temperature ranges.
Operating conditions are:
Input voltage: 24-60 V
Nominal Voltage: 48 V
Output voltage: 12 V
Output current…
Part Number: LM5010A-Q1 Tool/software: WEBENCH® Design Tools Hello,
I would like to know what is more reliable and efficient in terms of design reference: Webench online software or online calculator provided by TI.
Because when I was designing using…
Part Number: LM5010A Team,
My customer is looking for additional details on datasheet specs:
One of the parameters I’m looking at is the UVLO that occurs at 5.25V. The 5.25V is a typical datasheet value and I’m interested in the range or distribution…
Part Number: LM5010A Hello,
My customer is using the LM5010A buck converter, 48Vdc to 3.3Vdc. The 48Vdc VIN is also used for Power over Ethernet out RJ45 port. The board fails EN55032 Telco Conducted emissions tests at the 1.8MHz, the same frequency as…
Part Number: LM5010A Hi,
I would like to know how you can guarantee grade 0, that requires +150 degrees AMBIENT temperature and the datasheet specifies +150 degrees JUNCTION as max.
In this situation the device should have 0 W power dissipation.
Than…
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010A , hi team
can I know the Min On-Time to calculate Max allowable Fsw at max Vin ?
further, LM5010A and LM5010A-Q1 have same Min On-Time ?
Part Number: LM5010A Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi,
Is it possible to get hold of an LTSpice compatible model file for the LM5010A? The only model available is in encrypted PSpice format.
Regards, …