Part Number: LM5010A Other Parts Discussed in Thread: LM5010 Hi,
Because R&D needed wide input range DC-DC converter, R&D refereed to the application note AN-1352(snva101a).
On this document, there is a example input voltage range 12V to 75V.
…
Part Number: LM5010A Other Parts Discussed in Thread: LM5007 Hi,
We are woundering if we can set the current limit of LM5010A to below 1A, any way to do it ?
Thanks!
PY Tsai
Part Number: LM5010A-Q1 Dear all,
Could you provide with FMEA documents of LM5010AQ1MH?
My customer wants these information.
Could you provide three condition documents? (pin Open, pin to pin short, GND short)
Best regards,
Other Parts Discussed in Thread: LM5010A Hello furum members,
I am designing the main power supply of my microcontroller system with the LM5010A. I would like to have at the output: 12V and at least 1A. Please let me know if this combination can deliver…
Yamamoto-san,
Since the LM5010A-Q1 is a non-synchronous converter, there is no shoot-through current as defined conventionally using high-side and low-side MOSFETs in a synchronous buck converter. Also, if the freewheeling diode is a Schottky, the reverse…
Other Parts Discussed in Thread: LM5010A , LM5017 , LM5010 Hi,
can the L M5010 or LM5010A be used as a fly-buck converter?
In my case Vin=36V(18-72V), Vpri = 15V (200mA) Vsec = 5V(400mA)
If LM5010 does not meet the demand if I can use LM5017
Kind regards …
I would like to confirm the operation of the ripple rejection in the datasheet Figure 17.
1. Does the ripple at FB point increase by the increase of output ripple?
2. Can we use the ceramic capacitor of output capacitior for Figure 17 (C2)?
Best regards…