Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010 Hello All,
Simulation using Pspice for Ti. Buck regulator with part LM5010A-Q1
Facing problem with convergence error. Let me know how to resolve.
Part Number: LM5010A-Q1 The datasheet does not state how the exposed pad (underside) is electrically connected. Is it possible to connect this pad to GND (same as DAP, SGND, RTN)?
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LMR36006 , LMR36006-Q1 , , LM5010A Hello,
I would like to know what is Quiescent Current of this IC, as it is not stated in the datasheet.
Operation conditions are: Vin=36-60V; Ioutput=0.7A;Fswitching…
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010 Hello,
I am after LM5010A-Q0, which is the same part but has higher temperature ranges.
Operating conditions are:
Input voltage: 24-60 V
Nominal Voltage: 48 V
Output voltage: 12…
Part Number: LM5010A-Q1 Hi Team, We have a customer that go through this article:
How to dynamically control the output voltage with a COT regulator
Constant-On-Time (COT) regulators provide a simple , cost…
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010A , hi team
can I know the Min On-Time to calculate Max allowable Fsw at max Vin ?
further, LM5010A and LM5010A-Q1 have same Min On-Time ?
Part Number: LM5010A-Q1 Tool/software: WEBENCH® Design Tools Hello,
I would like to know what is more reliable and efficient in terms of design reference: Webench online software or online calculator provided by TI.
Because when I was designing…
Part Number: LM5010A-Q1 Other Parts Discussed in Thread: LM5010 Hi Team
customer made board with the below parameters;
- Fsw = 424Khz(Ron = 100Kohm),
- external ESR = 4.7ohm, Cout = 4.7uF
- Vout = 5V(Fbb = 5.1Kohm, Fbt = 5.1Kohm)
- Cff = 1nF…
Part Number: LM5010A-Q1 Dear all,
Could you provide with FMEA documents of LM5010AQ1MH?
My customer wants these information.
Could you provide three condition documents? (pin Open, pin to pin short, GND short)
Best regards,