Part Number: LM5025 Other Parts Discussed in Thread: UCC28056 , UCC2897A , UCC28180 I a looking for a controller that can work best with this topology: 120–277 VAC → PFC → 400 V bus → 48 V / 260 W active-clamp forward. I am lookiing at using LM5025: Active…
Part Number: LM5025 Other Parts Discussed in Thread: UCC2897A we are desiging new product DC-DC convertor using LM5025 controller. have simplis simulaion module of LM5025? or suggest any other controller for DC-DC convertor. We are targetting Active clamp…
Part Number: LM5025
I want to create a converter based on www.ti.com.cn/.../snvu096.pdf , but I can’t find the information about transformer T10 and inductor L10. Is there any alternative material available?
Part Number: LM5025 Tool/software: Hi,
I found a method to reduce the voltage spike on the secondary side diode of an active clamp forward converter and would like to apply it to the LM5025. Is this feasible?
His method uses diode rectification, while…
Part Number: LM5025 Tool/software: Dear Expert
100w Module
Exception description: Using LM5025CMTCX as the control chip and CS1 pin for short circuit protection, the CS1 voltage reaches the protection point of 0.5V during a short circuit, and the…
Part Number: LM5025 Other Parts Discussed in Thread: UCC28C43-Q1 , UCC28C53-Q1 , , UCC28C43 , LM5026 , UCC2897A , PMP21318 , UCC28951-Q1 , UCC2808A-1Q1 Tool/software: I am searching for forward converter driver IC. I want my input voltage in the range…
Part Number: LM5025C Other Parts Discussed in Thread: LM5025 Hi everyone,
I make a DCDC Buck converter with this schematic to provide, with input 48V, and exit of 24V.
With the LM5025, the converter starts to supply 24V at an input of 36V. This is…
Part Number: LM5025 the datasheet of LM5025 says to connect AGND and PGND as close as possible to the LM5025 pins.
PGND seems to be used only for the gate driver.
So if i use a current sense resistor between the (OutA) FET-S and Power-GND, why is…
Part Number: LM5025 Is there a detailed design proceedure for this LM5025 IC? The datasheet provides very limited information. The only design procedures I can find are for current mode operation but not this voltage mode active clamp forward converter…