Part Number: LM5032 Other Parts Discussed in Thread: UCC28220 By reducing the duty cycle via Rdcl, outputs 7 & 10 have a double pulse (sometimes triple) , never more .
Cres =100nF & Css= 220nF
Rdcl=68k ;
Rrt/syn =90.9k ;
Vin= Vcc= de 11 à 12V…
Part Number: LM5032 I have a customer who is trying to LM5032 to produce a high powered converter. See his remarks:
We are in the process of developing a 2KW Standby Power Inverter for Emergency Lighting. The main Power Board is comprised of:
A PFC Boost…
Part Number: LM5032 There was a previous answer that the LM5032 can also be used with DC input. How does the LM5032 operate when the input voltage of the LM5032 rises and exceeds the output voltage setting voltage DC 400V?
Part Number: LM5032 Dear all,
I have seen one module made using this LM5032 for Boost interleaved. and it worked.
Can anyone tell me if this balance current in both power stages.
It has separate current sense line and separate driver control unit. Only…
Part Number: LM5032 Hi,
Just want to check my understanding of how to adjust the slope compensation for the LM5032.
The datasheet states that adding resistance to the CS pin will increase the amount of slope compensation. So by adding a series resistor…
Hi
Thank you for your support.
For AC/DC models, LM5032 was recommended, but LM5032 input can be up to dc105v. Are you telling me to make AC/DC separately and use LM5032?
Thanks
Part Number: LM5032 Hi all Would you mind if we ask LM5032? On the datasheet Figure 9. Maximum Duty Cycle vs. UVLO Voltage, we can confirm Maximum Duty Cycle vs. UVLO Voltage. And then, there is the formula which is relation to RDCL and RT. -Maximum User Duty…
Part Number: LM5032 Other Parts Discussed in Thread: TIDA-00200 Dear Sir/Madam,
With the TIDA-00200 Reference Design, I am now testing the channel 1 of the LM5032 chip with the Channel 2 disabled purposely without the feedback loop (I just want to see…
Part Number: LM5032 Other Parts Discussed in Thread: TIDA-00200 , UCC28740 , LM5021 Dear Sir/Madam,
In TIDA-00200 "120 VAC, 200 W, 90% Efficiency, Interleaved Flyback for Battery Charging Applications Reference Design", it says the whole design will work…
Part Number: LM5032 Other Parts Discussed in Thread: TIDA-00200 Dear Sir/Madam,
I read the TI Design TIDA-00200 and want to buy components to duplicate this design. But in the file "tidra06", which is the BOM for TIDA-00200, I can not understand the part…