Part Number: LM5041EVAL Dear Sir,
Could you please share the gerber file for the LM5041EVAL board (AN-1299) so that I can see the PCB layout with more clarity.
Regards,
Nesh
Part Number: LM5041EVAL Dear Sir,
LM5041EVAL board is having a feedback circuit with some more additional components compared to the basic feedback circuits. I am having following doubts regarding components:
1. D12 maybe used for clamping the voltage…
Part Number: LM5041EVAL Other Parts Discussed in Thread: LM5041 , , LM5102 , LM5101 Hi Sir,
LM5041 has a feature of programmable dead time or overlap adjustment for Push Pull.
Do we have any option to adjust the dead time of buck stage (HD and LD pulse)…
Part Number: LM5041EVAL Hi Sir,
Keeping a (10E) resistor parallel to the diffrential mode inductor L1 (10uH) is mandatory or what is the practical advantage of the resistor in the circuit.
Part Number: LM5041EVAL Other Parts Discussed in Thread: LM5041 , Hi Team, My customer considers to use LM5041 and asked the following question. Is there efficiency data of LM5041EVAL? I would also like to have thermal data if there is. Best Regards, Yaita /…
Part Number: LM5041 Dear Sir,
Could you please share the specification output ripple % considered for the output 2.5V 50A in LM5041EVAL board.
how is the output capacitor value calculated 932uF (Total Output capacitance) with required ESR.
Thanks & Regards…
Part Number: LM5041 Dear Sir,
The transformer used in LM5041EVAL board is having 1.25mH primary inductance. (Np :8T, Ns: 1T)
in LM5041 the input is 35V-70V then after buck stage it'll be around 22V then current fed push-pull stage, which is having transformer…
Part Number: LM5041 Dear Sir,
The total input capacitor used is 8.8uF (2.2uF x 4Nos) for a input of 140W (approx) in the LM5041 EVAL board.
Could you please explain the input capacitor calculation for this configuration.
Thanks
Nesh