Part Number: LM5067 Other Parts Discussed in Thread: TPS23521 Hi Team,
Do we have a device that have lower threshold voltage of Current Limit/Breaker than LM5067? Customer uses 0.2-0.5mohm shunt and load current is about 70A, 50mV threshold voltage is…
Hi
A solution is needed to change the polarity of the output voltage.
Because the properties vary depending on whether the product is a positive or negative power source, you must change the polarity as desired.
Spec
Input: +42V
Output: 42V_100w(Depending…
Part Number: LM5067 hi expert,
lm5067 datasheet shows Fault detection current range is [140, 44] uA.
while another picture shows Fault detection current has little influence by temperature.
so above [140,44]uA range is mainly influence by design or chip…
Part Number: LM5067 Hi,
We are using LM5067 for a -48V, 10A system as per the following image. Please advice me that our circuit works as expected. Main requirement is to protect the system from accidental input reversal. Added two NMOS with a single…
Part Number: LM5067 Hi,
I have a question regarding the LM5067-2 insertion delay. Is there any other condition that can trigger this delay, other than the POR / VCC going high ?
Part Number: LM5067 Hi Team
We are planning to Load transient test with minimum and maximum load to validate LM5067. How can we do this? Can anyone suggest?
Regards
Srikanth Kacchu
Part Number: LM5067 Hello,
The device of LM5067 has the model number of LM50672NPAR, but there is no information in the data sheet. What is the difference between LM50672 and LM5067-1 and LM5067-2? Also, is the LM50672 either Latch-off or Auto-retry?
Best…
Part Number: LM5067 Other Parts Discussed in Thread: TPS23521 , TPS2399 Hello Ti
I am going though a inrush problem with BMS . By using a resistor to pre charge the load require the high wattage resistor or in case where load is short circuit the resistor…