Part Number: LM5106 Other Parts Discussed in Thread: LMG1025-Q1 Hello, LM5106 is being used for the motor driver. The problem is that LM5106 is burning.
There is a problem that GND is shaken because there is a mistake in the artwork.
By the way, I'm…
Part Number: LM5106 Hi,
In the datasheet I found:
"The LM5106 is a single PWM input gate driver with Enable that offers a programmable dead-time. The dead-time is set with a resistor at the RDT pin and can be adjusted from 100 ns to 600 ns. The wide…
Part Number: LM5106 I'm using a LM5106 to drive a half bridge but the high side seems to be shutting off in a very strange way.
It turns off well until it gets to the supply voltage; it then holds at supply voltage for approximately 50ns and then continues…
Part Number: LM5106 fault phenomenon:In the process of motor rotation, there will be a brief jitter. It is found by oscilloscope measurement that the MOS on the high side sometimes cannot be opened normally, and the duration is about tens of milliseconds…
Part Number: LM5106 Other Parts Discussed in Thread: LM5102 We are having problems with using LM5106 half bridge driver IC, it works most some of the time. but there are other times where we are seeing a lot of failures and excess IC temperatures. We…
Part Number: LM5106 Hi TI,
I have a buck converter during start up showing -6.6V at HS pin to COM pin. All traces is direct and short to reduce the parasitic inductance. However, there is still visible undershoot of around -4V across the bottom MOSFET…
Part Number: LM5106 Other Parts Discussed in Thread: LM5105 , , LM5104 Hi team, my customer is looking for an alternative to LM5105 due to supply issues. One alternative is LM5106, which does not have the bootstrap diode integrated, so it seems that it needs…
Part Number: LM5106 Hi,
I will design audio classD amplifier.
So I'm looking for a gate driver with a withstand voltage of 80V or more.
(I'm not going to use TI's one-chip class D.)
From your HP, I'm wondering if the LM5106 can be used. I…
Part Number: LM5106 Other Parts Discussed in Thread: UCC27282 , LM5164 Hello,
I'm working on a proof of concept for ultrasonic application using a class D amplifier made from 'discrete' parts.
We build a first prototype pcba wich embedds LM5016…
Part Number: LM5106 Recently, lm5106 was used to design the half bridge driver of the motor. The driver drives a 600W motor with 500 rpm. When the power is cut off for the whole machine, the upper tube of the board bridge driver is damaged; After measurement…