Part Number: LM5107 Tool/software: hi Team,
customer ESD standard is 2Kv HBM mode, but we are seeing the spec have a comment on few pin at 500V.
is that means the Pin 6 , Pin 7 and Pin 8 are rated at 500V HBM mode only ?
why not have two line, pin…
Part Number: LM5107 Other Parts Discussed in Thread: UCC27624 Hi,
Is it possible to connect HO and LO to the FET with GND reference as shown in the attached diagram?
Thanks,
Conor
Part Number: LM5107
The schematic is like this:
The following picture shows the input signal to the gate driver. Yellow is input of high side, Green is input of low side from mcu.
In the following picture yellow is the input of high side and…
Part Number: LM5107 Theres been a random failure in a BLDC Motor driver unit that comprises of The unit: A motor driver PCB (Microcontroller, Predrivers, 3 legs of N chn FET's) along with a BLDC Motor. Topology: 3 phase full bridge (all NChn FETs driven…
Part Number: LM5107 Hi Team,
I have a customer evaluating the LM5107SD and seeing an issue where the LO pin is latched high whenever VCC is supplied to the board despite changes to the LI pin. Is there any known instance where the outputs would remain…
Hi Richard,
Thank you for responding. Do we have any other alternative which is a direct replacement, pin to pin compatible with the same footprint of LM5107MA/NOPB?
Part Number: LM5107 Dear e2e support,
My customer is facing some noise issue with his design incuding our LM5107.
It's driven through a 25Khz PWM.
Has you can see below, we don't see any over/undershoot which could cause some EMI.
Most of the…
Part Number: LM5107 Hi Team, Is there any temperature variability data about tMON and tMOFF? It seems the following MAX values are under 25C. Best Regards, Yaita / Japan disty
Hi Richard,
Scrolling through our E2E posts I noticed that this post was not answered, our apologies!
The shorted external rectifier will carry almost all the current and you will have VDD = VHB.
If the external diode shorts, the bootstrap resistor…
Other Parts Discussed in Thread: LM5107 Hi TI,
I need your help. Can you give me the true table for LM5107? The true table should include HI, LI, HO, LO.
Thanks,
Don