Part Number: LM5109B Other Parts Discussed in Thread: TIDA-010042 , LM5109 Good day, We are using the LM5109 driver solution in interleaved buck converter design (see attached schematic). We used TIDA-010042 as a reference, just FYI. Apart from the buck operation…
Hi Shiv,
Thank you for reaching out! I would recommend simulating your circuit on PSPICE for TI with the LM5109 B PSPICE transient model from the LM5109B product folder page :
Using the simulation file, you can input your specific circuit conditions to…
Part Number: LM5109B Other Parts Discussed in Thread: LM5109
Dear Support,
I would need some help in a LM5109BMA Half-Bridge Converter design.
The LM5109 mounting: 2x PWM signals control the LM5109BMA inputs which drives 2x Power MOSFET (Idmax = 56A) and…
Part Number: LM5109B Other Parts Discussed in Thread: LM5109 I am having troubble using your product as a high side NMOS switch in my design.
High-side gate driver output does not work as stated in datasheet. The voltage on HO pin does not rise above Vin…
Part Number: TMS320F28065 Other Parts Discussed in Thread: CONTROLSUITE , DRV8312 , LM5109 Hello TI experts,
I am going to drive a PMSM motor using foc algorithm. I have designed a board which contains a f28065 microcontroller. In order to do that I started…
Part Number: TIDA-010042 Other Parts Discussed in Thread: LM5109 , INA280 , INA240 , LM5009 , LM5168 Hi, I have solar panel with output 15Watt and open circuit voltage 111V. I need to interface with TIDA-010042. TIDA-010042 maximum input voltage is 15 V to…
Part Number: UCC2808A-2 Other Parts Discussed in Thread: LM5109 , UCC28085 , UCC28083 The half-bridge topology we use is shown in the following figure:
We have following questions: question1:The recommended supply voltage of LM5109BMA given in the datasheet…
Other Parts Discussed in Thread: LM5109 , LM5108 Hi team,
Do we have any suitable devices to compete AUIR2085S? Thanks.
www.infineon.com/.../Infineon-AUIR2085S-DS-vNA-EN.pdf
Part Number: DRV8432 Hello,
I'm upgrading a hand-made TEC driver and want to get some features/minituarization from purpose-built ICs.
We're looking at 15V-24V and 6-10A. 24V / 15A would cover pretty much everything, and 15V/6A covers over half…
Part Number: LM5106 Other Parts Discussed in Thread: LM5109 , LM5111 Compared to the LM5106, the LM5109 has two inputs - one for low side and one for high side. This means that it is "easily" possible to achieve three different drive options with the LM5109…