Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113
My question is on the
Lm5113 part , the Tmon and Tmoff shows a delay matching of 1.5ns typical max 8ns I have a few questions
What is the output impedance of the driver during that “dead…
Part Number: LM5113-Q1 Other Parts Discussed in Thread: LM5113 Dear,
We chose LM5113 as the gate driver for GS1008P in our class-d audio amplifier (CDA), and there's a phenomenon we can't explain. We think the gate driver may cause it. Our CDA…
Part Number: LM5113 Other Parts Discussed in Thread: LMG1205 Hi!
I would like to know whether LM5113 is suitable for acting a RF amplifier for enlarge the NFC range application.
Thank you.
Part Number: LM5113-Q1 hi Datasheet says HS pin has -5V Abs max rating, is this DC ratings?
when the HS is pulled lower than -5V, what is possible damage? would it be ESD cell damage or different damage mode?
Part Number: LM5113 Other Parts Discussed in Thread: LMG1205 Hello,
I have a question regarding bootstrap for LM5113TME HB IC for GaN. As in the datasheet the LM5113 already have an internal bootstrap diode, is it recommended to use external bootstrap…
Part Number: LM5113 Hi,
I am working on a TINA simulation to use LM5113 for driving a synchronous boot converter.
The circuit is working fine and i am able to generate an output voltage.
But i am interested in understanding the bootstrapping current…
Part Number: LM5113 Other Parts Discussed in Thread: LMG1205 Hi team,
I have a customer design in LM5113 and confuse with how to connect the VDD and HS pin.
There have two pins of VDD and HS and should they open another one or they can short them.
Part Number: LMG1205 Other Parts Discussed in Thread: LM5113 , , LMG1025-Q1 , LMG1210
I have a few questions about GaN FET drivers such as the LM5113/LMG1205. Initial situation: Half bridges for inductive loads are to be controlled.
- Should Vss of the chip…
Part Number: LM5113 Hi,
I want to use the LM5113 gate driver to improve the performance of my class d amplifier. My input is a sin wave with frequency 20K and amplitude 2V. I built the circuit based on LM 5113 datasheet. However, when I do my simulation…
Part Number: LM5113 Dear Sir/Madam,
Based on the reliability data, shown this is a power Bicmos technologies node.
Is the fabrication based on Gan or SOI or SIGE materials?
Thanks
Regards,
Nick