TI E2E support forums
TI E2E support forums
  • User
  • Site
  • Search
  • User
  • E2E™ design support >
  • Forums
    • Amplifiers
    • API solutions
    • Audio
    • Clock & timing
    • Data converters
    • DLP® products
    • Interface
    • Isolation
    • Logic
    • Microcontrollers
    • Motor drivers
    • Power management
    • Processors
    • RF & microwave
    • Sensors
    • Site support
    • Switches & multiplexers
    • Tools
    • Wireless connectivity
    • Archived forums
    • Archived groups
  • Technical articles
  • TI training
    • Tech days
    • Online training
    • Live events
    • Power Supply Design Seminar
  • Getting started
  • 简体中文
  • More
  • Cancel


Search tips
Showing 161 results View by: Thread Post Sort by
    • 6/30/2020
    • Andrew Dunlop

    LM5119: Maximum values for current sense filter

    Part Number: LM5119

    Hi.

    I have some noise present on the CS and CSG pins of an LM5119 due to adjacent circuitry (another LM5119) switching at inconvenient moments.  They are synchronised, so it happens rather predictably.

    Adding a 1nF / 100R / 100R differential filter improved the situation dramatically, but there is some residual noise affecting the current measurement.  I know this because the input current draw changes (reduces) if the source of noise is removed.

    My questions are:

    1. What are the maximum permitted values for the differential current sense filter components?  I presume that the consequence of lowering the current sense filter bandwidth too far will be reduced accuracy / sensitivity to overcurrent conditions.  My switching frequency is 250kHz.

    2. Are there any other strategies for reducing the sensitivity to noise of the CS and CSG pins?

    Thank you in advance!

    Kind regards,
    Andrew

    Power management forum Power management
    • 10/27/2017
    • Ryuji

    LM5119: 4 phase operation with two LM5119s

    Part Number: LM5119

    Hello,

    Can we use LM5119 as 4 phase operation if we use external oscillator to RT input of LM5119 and 90° phase shifted clock input to other LM5199?

    Best Regards,
    Ryuji

    Power management forum Power management
    • 7/8/2020
    • Andrew Dunlop

    RE: LM5119: DCM with interleaved (single output) operation

    I'm very comfortable with CCM.  Thanks for your help.

    Kind regards,
    Andrew

    Power management forum Power management
    • 9/6/2019
    • David Kim6

    LM5119: Add OVP circuit.

    Part Number: LM5119

    Hi

    I am using an interleave circuit using the LM5119.

    The output voltage requires OVP.

    I'm trying to figure out what to do

    I want to add an OVP circuit. 

    Please let me know if you have a good idea.

     

    Power management forum Power management
    • 1/26/2018
    • Qian Chen

    RE: LM5119: How to approximate Error Amplifier Compensation network values for lm5119?

    Hello,

    LM5119 is emualted peak current mode controller. I think you can start with type 2 compensation. Type 2 compensation should work with low DCR inductor and low ESR output caps.

    Thanks
    Qian
    Power management forum Power management
    • 12/14/2017
    • David C

    LM5119: LM5119 Operation of the current limit when hiccup is disabled

    Part Number: LM5119

    Hello,

    When hiccup is disabled and the part is in current limit, will the part continue to operate in current limit indefinitely as long as the load is sufficient? 

    Regards,

    David

    Power management forum Power management
    • 5/14/2019
    • David Kim6

    LM5119: HICCUP mode

    Part Number: LM5119

    Hi

    I'm testing a dual BUCK(13V,18V) by LM5119.

    There is no problem with 13v but 18v start a hiccup at no load.
    Looking at the data sheet, there seems to be only an over current related to the hiccup.
    Can you be a hiccup for another reason?

    -test condition

    2-ch Buck(LM5119)

    1. Input: DC 66~100V

      Output: DC 13V / DC 18V

              DC 18V 1A(typ) / 11A(peak)

    Power management forum Power management
    • 8/29/2019
    • Aki Li

    LM5119: can it be used for constant current output?

    Part Number: LM5119

    Customer wants to use a controller for 12V input, <= 3V output, with 45A constant  output current. Can LM5119 achieve this? If not, do you have any other suggested parts? Thank you.

    Power management forum Power management
    • 4/11/2019
    • oulutek

    LM5119: 60V DC-DC Buck Controller Problem

    Part Number: LM5119

    Dear Madam or Sir,

    We have used LM5119 to design a buck converter from 16-60VDC to 12VDC. The target load current is 20A. The schematic is attached. And also the figure of the board.

    The test result is as follows.

    1. VIN=30VDC, VOUT=12V, Load=2A, board runs 15 hours without problem.

    2. VIN>30VDC, VOUT=12V, Load=2A, the output voltage changes from 12V to 8V and then comes back to 12V, and repeats in this way.

    Can you please give us some suggestions to diagnose?

    Board-SCH.pdf

    Power management forum Power management
    • 6/18/2019
    • Max Han

    LM5119: how to set VCCDIS pin and DEMB pin?

    Part Number: LM5119

    Hi 

    1. LM5119 is used in customer side, interleave buck, the output is 12V. so customer want that at start up, the internal VCC regulator is used, after 12V is stable, 12V is used to provide VCC power.

    On LM5119 EVM, a diode from output to VCC is inserted. customer want to know how to set VCCDIS pin (pin 8)?

    2. Diode Emulation Mode is not needed, so customer need to connect DEMB to VCC2. on EVM, this is a resistor R16, but this is no value shown.

    do customer need this resistor or connect to VCC2 directly? if R16 is needed, what's the recommended value?

    thanks.

    Power management forum Power management
<>

Didn't find what you are looking for? Post a new question.

  • Ask a new question