Other Parts Discussed in Thread: LM5119Q Dear Sir,
I want to design a 18-30Vin and 12V@30A DC/DC using LM5119Q. I dont see any Webench result but I've seen PMP7819. The input is 33-60V and the output is 12V@33A.
Could me any suggestion on what I should…
Hi Roy,
The LM5140-Q1 is a dual-channel controller that naturally provides 180 degree clock phase shift (this is the reason the LMC555 timer is added to the LM5116 reference design). You can also consider the LM5119Q 65V controller. If the max input…
Hello Dhimat,
We do not have any dual switchers with integrated fets rated to 40V.
Our dual integrated fet switchers, like TPS55386, are only good to 28V.
For single switcher with integrated fets see:
TPS54540 TPS54040A TPS54140A TPS54240 TPS54340…
Other Parts Discussed in Thread: LM5119Q , LM5119 Dear Specialist.
Our customer is considering to replace from LTC3890 to LM5119Q. They intend to design 4 phase interleave using 2 ICs. They shared each output of error amp to be same duty cycles in each phase…