Part Number: LM5155EVM-FLY Hi,
If my customer wants to start up the LM5155EVM-FLY Vin=4Vdc, will the EVM BIAS pin be modified to connect to Vcc?
Is there any directions for the LM5155X soft-start circuit? Thanks.
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM3481-FLYBACKEVM , LM3481 , LM5155 , Hi guys,
This is FAE supporting INOVANCE, which is the top 1 servo and AC inverter in China. I am trying to promote LM5155 to my costumer by comparing its performance…
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM5155 Dear Team,
My customer started LM5155 Flyback DC/DC application desing by using the LM5155/56 Flyback Controller Quick Start Calculator . They have a question at "Step 7: Loop Compensation…
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM5155 Let me ask you two questions: (1) I would like to design a 50W flyback converter using the LM5155. Is it possible to use the LM5155 in terms of power?
(2) Is there…
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM5155 Hi TI support :
Have this EVM board as Vin12 V and output 100V using transformer design ? i see your previous update , you are still planing in this beging of this 2020, now we will use…
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM5155 Hi,
Would like to test the LM5155EVM-FLY with 25 Vin and isolated 15 Vout, 75W . Do you have any suggestion on how to best modify the EVM?
Kind regards
Jorgen
Part Number: LM5155EVM-FLY Other Parts Discussed in Thread: LM5155-Q1 Hi,
I am planing to evaluate LM5155-Q1 for a Flyback converter. Vin 2V-12V, Vout 100V@0.01A.
See that you have a Evaluation Board. Can you please send me the Altium design files for…
Hi,
thank you for using the E2E forum.
You can have a look at the LM5158 (converter) of the LM5156 (Controller).
For both there is also a Flyback EVM available
LM5158EVM-FLY Evaluation board | TI.com
LM5155EVM-FLY Evaluation board | TI.com <- LM5155 same…
Hi Unnimaya,
Synchronous controller means the device has one low side and one high side switch. Asynchronous controller means the device has only one low side switch; the high side has a forward diode instead.
Latter controller is more common for Flyback…