Part Number: LM5156-Q1 Tool/software: hi,
am modulating the output voltage of the regulator the signal is a slow rising from 1V to 5V with a slope of 50Usec.
however, it rises correctly to the level with good control at full load of 500mA @ 35V, but…
Part Number: LM5156-Q1 Tool/software: Hello,
I have a design query that I need support with.
I'm using a LM5156QDSSRQ1 Voltage Regulator in a SEPIC Circuit.
we are observing an overheating SEPIC Inductor and an unexpected AC signal on the Voltage…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM5156 Hi Team,
I am simulating the LM5156-Q1 using Lt-spice but I am not getting the gate voltage in simulation.
Please can you check and let me know? What issue is the issue I am facing let me…
Part Number: LM5156 Other Parts Discussed in Thread: SN74LVC3G14 , LMG2100R044 , Hi
The circuit diagram is designed with the following specifications.
-SPEC-
Input: dc24V
Output: dc 80V 5A
Part: LM5156,LMG2100R044,SN74LVC3G14
I'd like to get a review, but…
Part Number: LM5156 Hello Experts, I create the desing to generate 90V using LM5156. I use the same design from the WEBENCH
I took this design and simulated in the LTSpice.
For some reason the Vout is 22V for LTSpice, whereas in the WEBENCH is 89V.
…
Part Number: LM5156 Other Parts Discussed in Thread: LMR36503 Tool/software: I would like to design a boost circuit using LM5156.
VIN=10 - 42V
IOUT = 1A
VOUT = 48V, 36V, 24V
The thinking here is that I can use some FETs to modify the feedback resistors…
Part Number: LM5156 Tool/software: Hi Sir,
we specifition is INPUT12-60V, OUTPUT 12V/6A.
may we know this schematic is ok? if there suggestion or need modify please let we know and learn from you, thanks.
ISOLATED_DC_INPUT_LM5156 - 編輯PDF.pdf
AE-SFD25005_A…
Part Number: LM5156 hi sir
i would like to design a dc-dc power stage, spec as below, LM5156 is a right solution?
For Positive, +10V~+110V Vout programmable, 48Vin, Continuous 0~40V /2A, Transient 110V/2A
For Negative, -10V~-70V Vout programmable, 48Vin…
Hi Marsh,
I am glad to hear the behavior improved with larger capacitance.
There are no other required chances I see right now. For the next revision, a general recommendation is to place some additional footprints for output caps, gate resistor and RC…