Part Number: LM51561-Q1 Hey guys,
i wanted to simulate a Sepic with the LM51561-Q1. I have downloaded the unencrypted file, converted it for LTSpice, but LTSpice gave me an error:
u:1:g_u8_abmii1:
Syntax Error
5u*v(u1:u8_uvlo_ok) << >>}
T…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156 Hey Guys,
i want to simulate a sepic converter with the LM51561-Q1. I downloaded
Unencrypted LM5156-Q1 PSpice Transient Model Package (Rev. F) SNVMBV9F.ZIP (204 KB) - PSpice Model
There is…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM51561 , LM5122 , LM5170 , Hi,
The customer configured the schematic with the specification below. However, there is no output.
I don't think it's possible with WEBENCH test.
Is it possible…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5122 , LM51561 Tool/software: WEBENCH® Design Tools Hi Team,
A customer is considering LM51561-Q1 for their new project with the following specs:
Input 6 to 36V
Vout=2A@70V
The design is not getting…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM51561 , LM51561 seems to have some interesting features regarding Dual Random Spread Spectrum and external sync.
However I noticed that if external sync signal is fed, the feature will be disabled…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM51561 Hi Team,
We are working on a project where we would like an LM51561 in a boost SMPS to output either 20V or 30V. Which voltage the circuit produces is decided by the the system's MCU at start…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM51561 Hi
Below is our circuit, the the target output is Vout = 21.1V, 0.15A.
if we apply 26V to the input of this circuit from connector P1, what voltage will we see at VREG (Vout) ?
And will this…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156 , LM51561 Hi TI
I think this issue was raised before, and TI Thinks Resolved, but that doesn't help me.
I'm trying to simulate flyback circuit with LM5156 controller with LTspice. Would…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5155 Hello,
please, could someone help me with feedback compensation? What am I doing wrong, any RC value combination is not the right. Always some kind of feedback unstableness observed.
pwrd.…