Part Number: LM51561-Q1 hi, Sir
regarding of LM51561-Q1,
When vin=13.5 and 17, Iout=3A, Vout=20, long run is normal. When vin=8v and Iout=3A, Vout=20, the output voltage is powered off immediately. Does this have anything to do with the capacitance of the…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156-Q1 , LM51561 Tool/software: WEBENCH® Design Tools I am looking to use the LM5156-Q1 part as flyback topology for operating range of 30 to 60 with nominal 50V. Out put will be isolated 12V and…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156 In this excel the Power loss analyzer doesn't work, the chart is not recalculated/redrawn.
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156 Hi,
I'm trying to simulate flyback circuit with LM5156 controller with LTspice. Would it be possible to get unencrypted spice model?
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM51561 , LM5156 Dear *,
we want to use LM51561 in two possible configurations with input power limit circuit ( using SS or other pin) and adjustable output voltage.
Configuration 1)
LM51561 in…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: TINA-TI , LM51561 Hello,
Using TINA-TI spice simulator i tried to do: Tools -> New macro Wizard, as i have done multiple times with unencrypted spice models. However this time i got the error:…
Part Number: LM51561-Q1 Other Parts Discussed in Thread: LM5156 I have created the schematics with Webench and the following settings:
Vin: 12V
Vout: 48V (at 1.5A)
I have noticed that Ccomp2 capacitor is 100nF. This is expremely high. In the demo board…
Other Parts Discussed in Thread: LP87563-Q1 , LM5143-Q1 , LM25141-Q1 , LM51561-Q1 , LM7480-Q1 , INA302-Q1 hi, Sir
Can your provide each parts excel design tool for LM7480-Q1, INA302-Q1, LM25141-Q1, LM51561-Q1, LM5143-Q1, LP87563-Q1 ?
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM51561 , LM5156 , UCC28600 , LM25180 Hi
I would like to design a QR-Flyback with LM51561H-Q1 SYNC-PIN.
The pri-Aux power will be the SYNC-single clock.
Will it work?
Could you offer the TI-Tina file…
Part Number: TPS54202 Hello,
I tried to import the device model provided as "TPS54202 Unencrypted PSpice Transient Model Package (Rev. C)" SLVMBJ5C.ZIP (102 KB) - PSpice Model. Unfortunately, this model is other than stated an encrypted version…