Part Number: LM51561H
Hi E2E Team,
We are using LM51561H as a flyback boost converter in our design. Below are operating conditions-
1) Input voltage: 18V to 32V
2) Output power: 65W (1.25A@54V)
3) Flyback Transformer: Attaching the transformer specification…
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM51561H
I am trying to make 100V using a SEPIC topology. If LM51561H is to be simulated using the WEBENCH of TI, it shows that it can be output up to 60V with a SEPIC topology. is this right? …
Part Number: LM51561H Hi team, I'd like you to review my schematic. If yes, I want to share it on a private message in E2E. Thank you for your cooperation. Sincerely. Kengo.
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM51561H , LM5156H , LM5156H-Q1 Hi Team,
My customer is using LM51561H-Q1 for refrigerator project.
Please review the schematic.
Input : Battery 10.5V~16V(Max 32V)
Output : 12V, 3A↓
LM51561H-Q1…
Part Number: LM51561H Other Parts Discussed in Thread: LM5155 Hello,
I power on for first time new DC/DC step-up from 24V to 100V.
At the moment load is 50kohm resistor, it will be an RC load, approssimately 200kohm in parallel with 100nF.
It seems working…
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM5156 , LM51561 Hi all,
I would like to develop an Boost converter using LM51561H-Q1.
The input voltage is 24V, the output voltage is up to 150V @5A .
Are these specifications compatible with…
Part Number: LM51561H Hi team, I'd like to know the Absolute maximum rating current for the BIAS pin. My customer sees a 1A peak current on the BIAS pin. Sincerely. Kengo.
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM5155 , LM5156 I am reviewing a suitable Device for the sepic converter. Could you recommend a suitable device and schematic for the following specifications? Vin = 12V Vout =+/-100V iout = 0.04A(max…
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM51561H , LM5156H Hi
Please review the customer's schematic
1. In the case of EVM, Out Put GND is to be Isolated. Is there any problem with the schematic layout?
2. In case of D1, it is designated…
Part Number: LM5156HEVM-FLY Other Parts Discussed in Thread: LM51561H , LM51561 , LM5156 Tool/software: Hello all
What is the Overload current of the part LM5156HEVM-FLY Evaluation Module?
i.e Output overload protection current of the same part
Regar…