Part Number: LM5161 Other Parts Discussed in Thread: LM5160 Tool/software: Hi! sir:
Is there any minimum load requirement of LM5161? If yes, how large it will be? Any equation or formula describes it?
Thanks,
Part Number: LM5161 I downloaded the LM5161_TRANS.lib spice to simulate on my board the LM5161 with LTSpice SW .
I got an error
Please see picture attached
Regards
Part Number: LM5161 Hi,
I used the Workbench to create a schematic of a buck converter, for a 10V output (with input ranging from 22V to 60V). I noticed, there are two NC pins. While one of them is not connected in the schematic, the other one is connected…
Part Number: LM5161 As shown in Figure 1, it is a BUCK circuit with a positive input and a positive output, with an input of 80V and an output of 3V; Is it possible to achieve an output voltage of -77V by swapping GND and input positions as shown in Figure…
Part Number: LM5161 Other Parts Discussed in Thread: SN6505B Hi experts.
I calculated the input capacitor to be 3.3u and 0.1u using the formula in the data sheet,
but the spike noise on the input side is about 1.5V.
Installing a larger capacitor will…
Part Number: LM5161
Dear Expert
Below is waveform measurement data on actual circuit application of LM5161PWPT.
-the abnormal 20V peak voltage was occurred on pin-10 (VCC pin) when hot plugging process (power on input DC voltage to input pin-3 of LM5161PWPT…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 I am designing a variable output voltage converter. The input voltage range is 20 - 50VDC. The output is variable from 0V to 12V @ 0.5A. Is the LM5161 a viable candidate for this design or…
Part Number: LM5161
Hello E2E Experts,
Good day.
Similar to LM5161 but something with 500uA or less would be ideal since I have a battery-powered device.
Thank you in advance for your support.
Regards,
CSC
Hi Marc,
I haven't heard back from you for some time so assume this issue is resolved.
Feel free to post a reply if this is not the case.
Regards,
Harrison Overturf