Part Number: LM5163 Hello, are there any differences between LM5163 and LM5163-Q1? Customer needs to test LM5163 but only LM5163-Q1 are in the sample room. I wonder because there are 2 datasheets.
Regards, Holger
Part Number: LM5163H-Q1 I developed a prototype, related to the datasheet, I measured a very high Vpp ~800mV, what can be wrong ? I have used the schematic in the datasheet with an inductor from WE 74404084121
Read more.
Part Number: LM5163-Q1 Hello team,
one of my customer does not use UVLO of LM5163-Q1. Will 47k ohm work as a pull up for EN from VIN?
What is the current required to drive this pin? What is the abs max?
Please share the details for driving such…
Part Number: LM5163-Q1 team, can you please advise the way the inductor is calculated in order to help my customer minimize value and size of inductor for operating point below:
Vin 30-60, Vout 12V iout .1-0.05A
Olivier
Part Number: LM5163-Q1
Hi,
The questions is related to the ISO 16750 standard where there is a momentary drop to 4.5V. How would the output react to the voltage drop?
Thank you
Part Number: LM5163-Q1 Dear team,
Could you let me know what is the leakage/input resistance of the EN/UVLO pin of LM5163-Q1 ? As far as I can tell, I don't find the information in the datasheet.
Many thanks in advance for your support!
Best regads…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163 Dear team,
I just wanted confirmation I understood how the PGOOD output of LM5163 is working, can you help me confirming below ?:
EN/UVLO < 1.1V --> Shutdown / PGOOD comparator is not…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163 Hi Team,
I received the following request, could you assist?
####################################################
We use LM5163-Q1 to convert the battery 24V into regulated 5V.
The…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5164-Q1 , LM5163 Dear,
our client was use LM5163-Q1, also we fill up excel file as attached, than we find some question as below:
1. we saw the LM5164-Q1 EVM , C8=33uF, But we use excel tool…
Part Number: LM5163-Q1
We are developing an automotive grade BMS. For that we need help with our design to make it comply with EMI EMC guidelines. Can you please share the mail id i need to review the ckt and Gerber file,...