Part Number: LM5168 Other Parts Discussed in Thread: LM5017 , , LM5169 Hello, I am designing a Flybuck converter with three outputs, spec as follows : 1. Input: 20 – 60Vdc 2. Outputs : (a) Non-isolated(main) 5Vdc, 50mA with LDO to get 3.3V …
Part Number: LM5168 Hello,
For the Iq given in the datasheet, this is non-switching Iq be it given for FPWM or PFM, correct? And not Iq (switching)?
Thanks!
Best,
Jacques St. Louis
Hi Aryan,
Since there is no update from your side after three weeks, may I assume the issue is resolved and we can close this thread? You can re-open it by adding a new post.
Thanks,
Youhao
Hi Allen,
Since there is not updates for 4 weeks, may I assume the issue is resolved so I can close the thread here? You can re-open it by adding a new post.
Thanks,
Youhao
Part Number: LM5168 Hi team,
Do you know if it's possible, and if so how, to extend the input voltage range for this part? Like extra external circuitry? My customer needs something that extends to 400V input range. Full details are 20-400V, output…
Part Number: LM5168-Q1 Hello E2E,
e2e.ti.com/.../3877515
I'm coworker with Kengo. Kengo has not to received reply mail about RTM schedule. Can I have information about RTM schedule?
Regards, ACGUY
Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5163H-Q1 ,
Hello,
There's no UltraLibrarian entry for this part yet (SO PowerPad DDA package). Is there a document with the PCB footprint data or perhaps an alternative UltraLibrarian entry we could…
Part Number: LM5168-Q1 Hello,
We’re developing an internal power supply for a PEV application that uses 10S-16S standard Li-Ion packs.
Input voltage to the supply will be 30V-67V.
Output voltage is 3.3V.
Load current is 0.5A-40mA, typically around…