Part Number: LM51772 Tool/software: Hi TI expert team,
has anyone ever operated the LM51772 with low voltage GaN HEMTs as external MOSFETs? If so, at what switching frequency and what input and output values?
Because I would like to try this, but the…
Part Number: LM5176 Other Parts Discussed in Thread: LM5177 , LM51772 , LM5175 Tool/software: Hi TI team,
Could you please share the comparison table for LM5175, LM5176, LM5177 and LM51772? Thanks.
BR
Sean
Okay, thank you Stefan. So, according to your answer, we can use the PSM-PCM-Mode for one direction of the energy flow, and the fPWM-Mode for the reverse direction. We wanted to build the whole system in multi-phase-operation (in our case, using two LM51772…
Part Number: LM51772 Other Parts Discussed in Thread: LM5175 , Tool/software: Hello Experts, Would you tell me the operating current spec? LM5175 datasheet is stated this spec as shown below. Best Regards, Fujiwara
Part Number: LM51772 Tool/software: Hello,
Can you tell me what the value for td(nFLT-PIN) is ? Is it 20us ?
Is there any waveforms showing the fault behavior ? thanks!
Part Number: LM51772LM51772-SCH.pdf
Hello,
A schematic was created using the LM51772, as shown in the inserted PDF file.
The input voltage /current :
Vin (min) = 12V;
Vin (noml) = 24V;
Vin (max) = 36V;
Iout (max) = 6A.
1. In the design schematics, the…
Part Number: USB2ANY Other Parts Discussed in Thread: LM51772EVM-HP , , LM51772 Tool/software: I'm pissed atm, I ordered the USB2ANY with my LM51772EVM-HP so I can directly test my use case without designing a prototype. I tried to connect everything…
Part Number: LM51772 Tool/software: The datasheet doesn't appear to indicate what the internal voltage divider ratio is between VIN and the values used when configuring VDET.
The voltage divider is shown on Fig 7-15.
Part Number: LM51772LM51772-SCH.pdf
Hello,
A schematic was created using the LM51772, as shown in the inserted PDF file.
The input voltage /current :
Vin (min) = 12V;
Vin (noml) = 24V;
Vin (max) = 36V;
Iout (max) = 6A.
1. In the design schematics,…