Other Parts Discussed in Thread: TINA-TI Hello,
I'd like to perform simulation of LM536035-Q1 in FPWM mode on the Webench, but it seems that only AUTO mode is available currently. How can I perform the simulation in FPWM mode?
Best regards, Shinichi…
Hi All,
The data sheets are listed as follows.
(4) The maximum recommended output voltage is 6 V. An extended output voltage range to 10 V is possible with changes to the typical
application schematic. Also, some system specifications will not be achieved…
Other Parts Discussed in Thread: LM53603-Q1 , TPS54060 , LM53603 , LM536035EVM Can someone make an educated assumption about tr an tf of LM53603-Q1? Their values affect IC Power dissipation. For example in Application report SLVA317B the author made an assumption…
Other Parts Discussed in Thread: LM53603-Q1 , LM53603 Dear support team
My customer evaluate LM53603-Q1 using EVM.
In frequency response data, Gain prot starts from 0dB at Vout=3.3V Iout>1A (see attached file.)
Is this normal operation?
Could you adovise…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM53635-Q1 , LM5018 , LM25141-Q1 , LM53603-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] According to the datasheet, the operating lifetime is de-rated for…
Other Parts Discussed in Thread: LM53603 Hi,
Mycustomer has three questions about [9.2.2.6 BIAS] of LM53603 datasheet. =======================================================
Q1. Is it possible to Vout is BIAScurrent any 3.3V or 5V is below 100mA by adding…
Part Number: LM43602-Q1 Other Parts Discussed in Thread: LM53602-Q1 , LM43602 , LM53603
Hello,
I'd like to ask some questions about LM43602-Q1.
At the input voltage of 6 to 6.5 V that will not rise further, will a LM43602-Q1 switch its switching mode…
Hi Gavin,
As far as calculating value for common mode choke is concerned there are number of tools available (from choke manufacturers) online that could be used to determine necessary value. This will depend on several factors, such as current rating…