Part Number: LM60 Hi E2E, Good day. Our customer would like to know what is the temperature-sensitive surface of the LM60 sensors since they need to measure the surface temperature of rock samples. Which part of the sensor would be better to put in contact…
Part Number: LM60 Other Parts Discussed in Thread: TMP235 , LMT84 hi dear supporting team,
understand that 130degree is beyond our characterization range, but customer still want to know, if the output voltage at 125degree is 1.205V, when the temp goes…
Part Number: LM60 Other Parts Discussed in Thread: LM45 Hello team,
Is there any solution as follows in PTC analog output temp sensors such LM60? - Can be set or adjusted to 0V output at 0C.
Thanks in advance. S.Sawamoto
Part Number: LM60 Hi Team,
It is planned to radiate heat from the device temperature rise to the copper foil of the PCB. In other words, multiple devices that heat up are mounted on PCB. Since the device temperature cannot be measured directly, we would…
Part Number: LM60-Q1 Hello Apps team,
My customer is asking minimum setup time of LM60-Q1 after supplying input voltage.
Figure 11 in datasheet shows output voltage which represents temperature is set within 5us after power supplied.
Vo is read…
Part Number: LM60 Hi Team, Our customer is requesting to have the Spice model for LM60 and the model is unavailable in the TI website. Can you share it here if possible? Thanks! Carl
Part Number: LM60 hi dear supporting team,
as for LM60 , the temp it reports is the brd temp or the Case temp of the chip itself? how is the precision of +/-4degree get?(comparing to which position temp ). and for room temp, the precision should be…
Part Number: LM60 hi dear supporting team,
as for LM60, the temp it reports is the brd temp or the ambient temp? how is the precision of +/-4degree get?(comparing to which position temp )
my customer is using it for detecting the temp in power module…