Part Number: LM60430 Hello,
We are using LM60430DRPKR and LM60430ARPKR. These chip are tough to get and have over 100 weeks lead time. We redesigned our PCB to include this chip as they are new chips. But suddenly they have just disappeared
Any recommendation…
Part Number: LM60430-Q1 When the values of components given in the data sheet are put into the simulation program they do not even come close to passing CISPR 25, and when I use just the simulation tool, minor changes cause erratic changes in other components…
Part Number: LM60430 Hi,
We are planning to use LM60430 in our design to convert 8-36V wide input voltage to 3.3V. We have two different BOM configuration, out of which in one configuration, the current requirement will be less than 3A. But n other one…
Part Number: LM60430-Q1 I have had one TI Power Designer design fail conducted emissions and attached is a second new design that uses the same parts as the evaluation board.
I need some assurance that this new design will pass conducted emissions testing…
Part Number: LM60430 Other Parts Discussed in Thread: LM43603
Dear *,
We are using LM60430D.
Vin= 12V to 24V
Vout= 5V
Iout_max= 3A
Please see the attached schematic if it looks good?
0574.Power Input.pdf
We also tried to add EMI filter in WEBENCH Power…
Part Number: LM60430LM60430 datasheet P19 is described that "a minimum of 10µF of ceramic capacitance is required", but the other EVM and reference schematic are used 4.7μF (and 220nF×2).
Please let me know about the background…
Part Number: LM60430-Q1 Hello team,
Due to a stock problem, my customer is considering LM60430-Q1 for their project. Their project uses the Raspberry Pi zero (1GHz) as their edge compute. They will use the LM60430-Q1 as a 24 to 5 V DC-DC converter. They…