Part Number: LM60430 Hi Experts,
I ran the Webench with below condition.
Device : LM60430A
Vin : 24V
Vout : 5.15V
Iout : 3A
Tj on Webench shows that Tj becomes 133.61 degC at 30 deg C room temp.
It looks so strange. Could you please check it?
Regards…
Part Number: LM60430 Hello, E2E
When no voltage is applied to VIN Is there any problem even if a voltage is applied to the EN terminal?
For example 0s: VIN = 0V, EN = 5V After 100millisecond : VIN = 20V, EN = 5V
Best regards, MITANI
Part Number: LM60430-Q1 rant rant rant
I do want to use a TI part, but I am not impressed that a TI part that is advertised as meeting CISPR25 standards still needs an input filter. I also find it very troubling that the values given in the data sheet…
Part Number: LM60430-Q1 Other Parts Discussed in Thread: LM60430 , LMR33630 Hi Team,
It appears that Webench won't simulate the LM60430-Q1. Any idea why this isn't working? Do you have any other suggestions for alternative devices that we could use to…
Part Number: LM60430-Q1 I'm trying to figure out how large of an inductor value can be used with the LM60430-Q1 when the max load current is under 500 mA?
Using Webench, it recommends 10 uH, while the Quick Start calculator reports 60 uH. I'm worried…
Part Number: LM60430 Other Parts Discussed in Thread: LMR33630 Hi,
I try to run the simulations provided on the webpag of the LM60430. I just download them then open the project and "click run".
I always get the following error:
"ERROR(ORPSIM…
Part Number: LM60430 Other Parts Discussed in Thread: TPS2116 Hi,
I use the LM60430 to do a step down converter : 12V to 5V / 2A. I need to add a super capacitor on the 5V power supply.
I would like to know if I have to add a serial diode between the SW…
Part Number: TPS62933P Tool/software: Hi support team,
I've got some only undershoot. The minimum voltage is -3.1V. The waveform is acquired at different times, but I attach magnified view.(With this waveform,the minimum voltage is -4.1V)
According…
Part Number: LM60430 Dear *,
can you tell is LM60430 a good choice to create Split-Rail converter like in SLVA369A application note?
Vin from 12V to 24V
Vout+ = 10V
Vout- = -10V
What is the max current that can be achieved in spilt-rail with LM60430 …