Part Number: LM60430 Dear *,
in the DS of LM60430DRPKR ( 1MHz) on page 20 it says that also 100-nF capacitors can be used for high frequency bypass is that also correct or is this a typo and 220nF must be used?
Best Regards,
David.
Part Number: LM60430 Hi,
I have to design a dc-dc based on the LM60430.
I would like to calculate the output capacitor and I am used to do it with the cut-off frequency of the loop. Here I do not have this information so I must use the formula given in…
Part Number: LM60430-Q1 Hello Guys,
Good day.
What is the power consumption rating for the LM60430AQRPKRQ1? It seems that this is not directly specified on the datasheet. Any estimated value/s?
Thanks!
Art
Part Number: LM60430 Other Parts Discussed in Thread: LMR33630 I have an application where I need the normal output level to be 5V. It is possible that in some instances the input voltage will drop to 4.5V. This may or may not be OK, depending on the IC…
Hi Frank,
I've also sent to you by message.
Seems LM60430 can only 3A output current, but in the waveform you sent to me, the input current is over 3A. So I think this Vin voltage drop is caused by the LM60430 current limit.
I'd suggest customer to…
Hello
I don't have visibility into what devices are in stock.
However, you might want to look at devices such as the LMR33620, LM43602, LM60430 or LM73605 family of devices.
Thanks
Part Number: LM60440AQEVM Other Parts Discussed in Thread: LM60430 , LM60440 Hi Team,
Can you have a look at below customer questions please?
I soldered my Evalboard LM60440AQEVM to 3.45V output voltage, started it, all good.
Now I started it again - days…
Murthy,
See two options below:
LM60430
Smallest package option
Enhanced QFN package for excellent thermals
36-V, 3-A rated
LM61440
4-A current rating for more flexibility
Similar features set to LT8609
Regards, Alejandro