Part Number: LM61440-Q1
while i'm simulating LM61440AAS-Q1 by in SIMatrix its taking more time to complete the simulation, can you please tell me how to reduce the run time?
Hi Songzhen,
Let's continue offline in the thread I had previously included you in.
I have no expertist on this matter so please ask for further feedback from the internal product engineering team.
As such, I will close this thread for now so we can…
Part Number: LM61440-Q1 Hi, What will be the minimum switching frequency when operated in Auto mode- Light Load operation: (PFM). Will it be less than 200 kHz.
Part Number: LM61440-Q1 Hi Experts
This device have standby mode and describe as below:
I don't know which application scenarios need to use this mode?
my customer want to know how to use this mode?
Part Number: LM61440-Q1 Hi Expert,
I see in LM61440-Q1 datasheet, that the recommended inductor value is quite large. Actually via calculation =1000*(1-Vout/Vin)*K/(Fsw*K*Iout), the calculated value is about 5.46uH instead of 8.2uH. May you help explain…
Part Number: LM61440-Q1 Hello, At Figure 10-42 of the datasheet, there are two plots called “Peak Signal” and “Average Signal”. What do you mean by the “Peak Signal” and “Average Signal” respectively? …
Part Number: LM61440-Q1 Other Parts Discussed in Thread: LM61440 Hi team,
Can LM51440 meet mission profile under below condition? (where Vin always on, and EN=L for 90% of time.)
EN=L
temp
-40
23
40
75
85
time(hours)
7227
24090
78292
9636
1204.…