Part Number: LM61440-Q1 Hi Experts,
LM61440-Q1 is D-win in customer side. Now it's mass production status. Could you share the acceptance Criteria for QFN package in our product line?
Due to the packaging type of QFN products, there will be residual…
Part Number: LM61440-Q1 Hi, What will be the minimum switching frequency when operated in Auto mode- Light Load operation: (PFM). Will it be less than 200 kHz.
Part Number: LM61440-Q1 Hi Expert,
I see in LM61440-Q1 datasheet, that the recommended inductor value is quite large. Actually via calculation =1000*(1-Vout/Vin)*K/(Fsw*K*Iout), the calculated value is about 5.46uH instead of 8.2uH. May you help explain…
Part Number: LM61440-Q1 Hi Experts
This device have standby mode and describe as below:
I don't know which application scenarios need to use this mode?
my customer want to know how to use this mode?
Part Number: LM61440-Q1 Hello, At Figure 10-42 of the datasheet, there are two plots called “Peak Signal” and “Average Signal”. What do you mean by the “Peak Signal” and “Average Signal” respectively? …
Part Number: LM61440-Q1 Other Parts Discussed in Thread: LM61440 Hi team,
Can LM51440 meet mission profile under below condition? (where Vin always on, and EN=L for 90% of time.)
EN=L
temp
-40
23
40
75
85
time(hours)
7227
24090
78292
9636
1204.…
Part Number: LM61440-Q1 Hi team,
Could you help to provide LM61440AASQRJRRQ1 1. TS16949 certificate 2. AEC-Q reliability report So that we can apply for the FXN vehicle specification part number.
Thanks
Part Number: LM61440-Q1 Other Parts Discussed in Thread: LM61440 I'm trying to create BUCK regulator using TI LM61440 with the next input
Input voltage 9 -16V
Case 1:
output : 5V@2A
At 2MHz switching frequency it works
When I'm trying to reduce the…