Part Number: LM61460 Other Parts Discussed in Thread: LM61495 Hi team,
Customer would like to design 12V input and -5.5V(6A) output. Can we use LM61460 to design it? Is there a reference schematic? Thanks!
Regards,
Alex
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 I'm trying to use Pspice for TI 17.4-2023 S009 Windows SPB 64-bit Edition to simulate the behaviour of LM61460-Q1. I have set the STEADY_STATE parameter to 1 and the simulation shows the…
Part Number: LM61460 To measure current during sleep, I would like to add 100mohm shunt resistor in below position (marked with red), and the measured by amplifier+ADC circuit.
Let me know if there is any risk for power supply control loop.
Part Number: LM61460-Q1 Hi, Please provide the following parameters for the conditions mentioned below for part: LM61460AASQRJRRQ
Condition: Vin=13.5V, Vout=3.3V, Iout=4.183 A, Fsw=480 kHz, Lout=4.7uH, Cout= 3*47uF
Parameters: 1) Rise Time and Fall time…
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM73606-Q1 Team,
We are trying to promote LM61460-Q1 against our own LM73606-Q1, as LM61460-Q1 is an advanced part. While could you also help to provide a comparison table to show their difference,…
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 Hi team,
Which model is the light-load high-efficiency curve of LM61460 tested on? The customer's test output VOUT=4V, Iout=6.4mA; input Vin=12V, Iin=6.1mA, switching frequency 1.911MHZ, so…
Part Number: LM61460-Q1 Hi team,
I have a question about inductor selection for LM61460-Q1. The datasheet said that to avoid subharmonic oscillation, the inductance value must not be less than 0.32*VOUT/Fsw . In my opinion, the subharmonic oscillation…
Hi,
I haven't heard back from you for some time so I will assume you were able to resolve this on your end.
Because of this I will be closing thread. Feel free to reply back to this thread so that it can reopen for further discussion.
Regards,
Ji…
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 hi expert,
There are some questions about the LM61460 working in unloaded mode, The output voltage at no load is higher than in normal mode, and I found the following explanation in…
Hi,
I haven't heard back from you for some time so I will assume you were able to resolve this on your end.
Because of this I will be closing thread. Feel free to reply back to this thread so that it can reopen for further discussion.
Regards,
Ji…