Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM61460-Q1 , , LM73606 , LM61460 Hi Team,
Can you please provide an in-depth (not high level product detail comparison) spec comparison between the LM73606-Q1 and LM61460-Q1?
Thank you in advance!
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61440 Hello expert,
Input 9~16V,output 7V 5A,power coil is 4.7uH,below is the schemitic
I want to test the output over current limit function of this device. But when I increase the Eload CC…
Part Number: LM61460
Hello expert,
For the datasheet I have some question below:
1.VOUT adjustable from 1 V to 95% of VIN——what is the input voltage and output power for this case?I test my board with Vo=7V and find the Vin min is 7.9V to ensure this…
Hi,
I haven't heard back from you for some time so I will assume you were able to resolve this on your end.
Because of this I will be closing thread. Feel free to reply back to this thread so that it can reopen for further discussion.
Regards,
Ji…
Part Number: LM61460-Q1 Hello expert,
We have a project where CV buck need to provide a LED board with linear CC driver.The LED board will implement a very complex PWM dimming( many CC driver dimming but not synchronous).
So are the three variant the…
Part Number: LM61460 Other Parts Discussed in Thread: LMR33630 , Hi,
I am confused why 6A LM61460 PG deglitch time is much lower than LMR33630's PG deglitch time? And why LM61460's rising deglitch time is much higher than LMR33630? Any consideration?…
Part Number: LM61460 Other Parts Discussed in Thread: PSPICE-FOR-TI Hi,
Here a project using LM61460, I am doing some simulation with this chip and its filter. I can't find the simulation model of this chip.
Could you help provide it ?