Part Number: LM61460-Q1
Hi Team, Our customer is considering to use a ferrite bead in place of the boot resistor for LM61460-Q1. Ferrite bead specifications are 500mΩ DC, 2.2K at 100MHz. Would this work the same, better, or worse when compared to the…
Other Parts Discussed in Thread: LM61460-Q1 Hello,
Regarding LM61460-Q1, is there any protection against reverse current when the OUTPUT voltage is higher than the INPUT voltage?
If not, what phenomenon could happen, and what kind of solution can we use…
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 , LMR23630 Hello,
How soon external clock can be applied after EN assertion?
My customer is facing start up problem with external clock being applied before EN. I also would like you to confirm…
Part Number: LM61460 Other Parts Discussed in Thread: LM61440 , LMR33620 In case if I set in WEBENCH POWER DESIGNER for LM61460 next :
Vin = 12 -32 V
Vout = 5V
Iout = 2A
WEBENCH says design can't be created. How to understand this report?
In case …
Part Number: LM61460
What this circuit does is that it takes a +/-15V as its input and generates an output from 12V to 30V at currents up to 1/2 Amps. The function of the circuit is to driver a heating element. I will send that photo as well.
The…
Part Number: LM61460 Hi team,
My customer is trying to evaluate auto version LM61460 instead of non-auto version due to the delivery constraint.
Could you please let me know what is the difference between auto and non-auto version (LM61460AANQRJRRQ1 and…
Part Number: LM61460 Hi
In the datasheet I see a comparison table for LM61460 which said that LM61460 does not have the function of spread spectrum:
But in the description of datasheet, it is shown below:
So a little bit confused about the function…
Part Number: LM61460-Q1 Hi team, Our customer is looking for the value of the Ramp-up time of LM61460-Q1 at 5V as it is not available in the datasheet. Can you share this information? Thanks, Jonathan
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 , LMQ61460 Hi Team,
There is a good new that DIN LM61460AASQRJRRQ1 !
Because of the material condition, customer is in urgent need of IC! Please help recommend a P2P solution (without need…
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM61460 Hi, teams!
I show an example circuit of LM61460.
but there is a difference between datasheet(Rev.F) and webbench.
Which circuit should I take?