Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 , LM62460 , LM61480 Hi I see in the datasheet that for the three part numbers: LM61495, LM61480, LM62460 they are rated for 6A,8A, and 10A, and are drop-in pin-compatible. However, I don't see…
Part Number: LM61480-Q1 Dear Team
Good day
Our customer use the LM61480-Q1 in their application , please help them them to review the schematic ,Please review it & provide feedbacks.
Wide_Input.pdf
BR,
Leon.liu
Part Number: LM61480-Q1 Other Parts Discussed in Thread: TINA-TI , LM61480 , PSPICE-FOR-TI , LMR43610-Q1 Our IT Department just installed TINA-TI on my laptop today 5/06/2022. I have several designs on the TI WEBENCH Power tool involving DC-DC converters…
Part Number: LM61480 Hello,
In this application, the customer will have either 12Vin or 24Vin and they need a regulator to buck that down to 12V, output current up to 8A.
If the input is 12V they don't need to regulate it we can just pass it through.…
Part Number: LM61480-Q1 Hi Team,
Our customer is looking for the footprint of LM61480QRPHRQ1. I have shared the footprint from the Ultralibrarian in the link below. However, he wants to cross verify if the footprint from the Ultralibrarian is correct.…
Hi Malakondareddy,
Are you on contact with a TI FAE for this application?
For the non-inverting buck-boost, take a look at the LM5175/6/7 family. And for 24V to 5V/8A buck stage, see the LM61480-Q1 8A converter.
--Tim
Hello Nico
The responsible engineer is out of office now. I will respond until he returns back. Thank you for your patience.
Please consider LM61480, and LM61495 if the maximum input voltage is <=36V. If VIN>36V, then ypou may have to use controller devices…
Part Number: LMQ66410 Other Parts Discussed in Thread: LM61480 , LM61495 , LM62460 , LMQ66420 , , LMQ66430
Hi support team,
Are the differences between LMQ66410, LMQ66420 and LMQ66430 the same as the differences between LM62460, LM61480 and LM61495?
・Current…
Part Number: TPS5450 Other Parts Discussed in Thread: LM61480 Is it possible to double the current capacity by bundling the two outputs of TPS5450?
Many LEDs have a common Anode, which requires a large current.
Please give me advice.
Part Number: TPS54561 Other Parts Discussed in Thread: LM61480 Referencing:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1226147/lm61480-q1--5v-inverting-output-possible
Current PCB uses TPS54561 for +5V…