Part Number: LM61495 Other Parts Discussed in Thread: PMP23333 , , TPSM63610 Tool/software: Hi support team,
I am looking for a device that can be used with the following plan.
Plan-1 Vin : 6.5V Vout : -6.5V Iout : 3.0A
Plan-2 Vin : 5V Vout : -5V Iout : 2.6…
Part Number: PMP23333 Other Parts Discussed in Thread: LM61495 , TPSM63610 Tool/software: Hi support team,
I am looking for a device that can be used with the following plan.
Plan-1 Vin : 6.5V Vout : -6.5V Iout : 3.0A
Plan-2 Vin : 5V Vout : -5V Iout : 2.6A …
Part Number: LM61495-Q1 Tool/software: Hi expert,
Can you help me test below case about our transient response in 2.1MHz sw frequency?
The normal idle current is 0.6A but peak current is 9.7A in 1ms, the voltage tolerance is 3.3 ± 0.15 V.
Thanks…
Part Number: LM61495 Hi,
i intend to use LM61495 for (15-32v 24 nominal) 24v-12v conversion at 0.6A\0.3A (max load\light load).
would you recommend this use? , could you estimate the efficiency of this solution? (using 400Khz switching frequency)
also…
Part Number: LM61495 Tool/software: Hello,
In our application, we need a MCU and DC-DC to make a adjust power supply unit with 36V input and 5-30V 10A dynamic output, and from https://www.ti.com/lit/an/slva861/slva861.pdf, we think we can use LM61495 for…
Part Number: LM61495 Hi team,
The data sheet has this description, and I'm a little confused. If we want to get the output voltage from 1V to 15V. Can we tie Bias pin to output? Because the output has more than 12V, as the DS said, we need to tie this…