Part Number: LM61495-Q1 As part of our design analysis we require following parameters of the Regulator IC LM61495QRPHRQ1
1. Trise, Tfall - low side MOSFET rise time and fall time
2. Forward direction voltage of low-side MOSFET body diode
Your fast response…
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 Hi Team,
Customer use LM61495 to change 12V to 5.5V.
If the input is lower than 5.5V, will output through/follow input, nearly 5.5V?
Part Number: LM61495-Q1 Hi. teams
The board I built with your help last time is working fine. Thank you. I have one question for you. Currently, the value of L43 is 2.4uH, but there is no stock in the market, so I wonder if it can be applied with 2.2uH…
Part Number: LM61495-Q1 Hi Team,
Could we provide the calculation of Cin/Cout for customer? The datasheet only give the recommendation value of these.
Customer want to calculate it to figure out the Cin/Cout so as to calculate the tool cost.
Part Number: LM61495-Q1 Other Parts Discussed in Thread: TINA-TI , hi,
i got a design from the webench, using the part: LM61495-Q1
i try to export it to Altium Designer (i have V21.0.8) but i don't have the possibility - the only export choice i have is…
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 Hi. Teams
I would like to apply LM61495QRPHT-Q1 to the project. I am trying to configure the circuit as below, but I have some questions.
- INPUT : 12V (Input range : 4V ~ 36V)
- Switching…
Part Number: LM61495-Q1 We are using LM61495QRPHRQ1 in our design
We would like to know how long the short circuit current will flow in the output section
1. as per dataheet image given below, if the short is removed with in wait time of hiccup the regulator…
Part Number: LM61495-Q1 Hi team
Could you review 3 schematics as attached?
Regards,
Noriyuki Tawkahashi LM61495Q3RPHRQ1_3.xlsx LM61495QRPHRQ1_2.xlsx LM61495QRPHRQ1.xlsx
Part Number: LM61495-Q1 Is the scheduled release for 4th quarter of this year still up to date?
Is there a more exact date now?
Is it possible to preorder manufacture samples?