Part Number: LM62460 Hello,
I measured the undershoot of the SW pin using the LM62460. Attach the waveform. It undershoots for a period of 6.4ns and drops to -1.83V. Looking at the description in (3) of the absolute maximum ratings in the data sheet, it…
Part Number: LM62460
Hi,
A quick question concerning LM62460. The SYNC/MODE pin Absolute Maximum Ratings is specified as min -0.3V and max 42V. But no further information in Recommended Operating Conditions.
Here we have a buck design with VIN 24V, we…
Part Number: LM61460 Other Parts Discussed in Thread: LM62460 Hello team, Could you please provide the comparison between the below mention I think in electrical characteristics all are same, please provide the difference between them Thanks and Regards…
Part Number: LM61495 Other Parts Discussed in Thread: LM62460 , LM61480 Hi support team,
Do LM61495, LM61480 and LM62460 have the same MOSFET?
Is it only the current limit that is different?
Is Figure 7-4 data for LM61495?
Is the loop stability adjusted…
Part Number: TIDA-020047
Hello,
This component LM62460QRPHRQ1 isn't available right now :
https://www.mouser.fr/ProductDetail/Texas-Instruments/LM62460QRPHRQ1?qs=QNEnbhJQKvYn1QEWk8lAhA%3D%3D
can I replace it by this one LM62460Q3RPHRQ1 and without…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 , LM25143 , LM61495 , LM25148 , LM61480 Hello team,
I’m looking at an apps note for “ Configuring LM62460 for Dual-Phase Operation “.
For more load sharing, is it possible to…
Hi,
Do you have a TI FAE contact that is supporting you? I can get in contact with them about this and they can help further assist the communication offline.
Regards,
Jimmy
Part Number: LM62460 Other Parts Discussed in Thread: LM61495 , , LM61480 , LM3489 , LM25148 Hi Team,
My customer is designing a 12~24Vin, 12Vout power, when 12Vin = 12Vout, they hope that the controller can close 100% duty(H side SW fully turn on) as possible…