Part Number: LM62460 Other Parts Discussed in Thread: LM61495RPHEVM , ,
Hi team,
my customer mistaken the Cboot connection as you can see in the schematic here.
they tried to re-work on the board with single-core wire ,
1. they first cut off the connection…
Part Number: LM62460-Q1 Good morning,
i have tried to do a simulation with webench of the power supply LM624606-Q1 , with these parameters:
vin: 16V-28V;
vout: 12V;
iout 6A.
Webench doesn't allow me to do this simulation, it tells me "Design cannot be…
Part Number: LM62460-Q1 Hi Team,
Does our LM62460-Q1 can be used in two parallel design? I see the risk one chip may trigger OCP, which will lead Vout drop. Pls share your opinions here.
If not, do you have some better solution to recommend for two 6…
Part Number: LM62460 Hi Team
My customer is looking for a regulator solution with Vout programmable in real time.
Vin: 24V
Current: 6A
Could you advice either integrated or discrete solution for this case?
Regards
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Dear teams,
My customer is using LM62460-Q1. I have checked the DS and function safety document, while it seems that this device does not have internal function safety diagnostic feature…
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Hi
im trying the attached circuit on my PCB: On my first PCB the circuit does not work as expected, i receive 2.8V rather than 5V and the reset pin is low indicating that the IC is fault…
Part Number: LM62460-Q1 Hello Team,
Are ICs able to work as an inverting buck-boost converter?
- LM61495QRPHRQ1
- LM61480QRPHRQ1
- LM62460QRPHRQ1
Thanks.
Regards,
Hirata
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 Dear TI,
I am working on the thermal design of LM62460 based converter and I have some questions regarding the IC thermal properties.
RthJB is given in datasheet and a note in layout chapter…
Part Number: LM62460
Dear Teams,
We are evaluating the LM62460 as a VBUS power supply for USB-PD.
Since the output voltage changes from 5V to 20V, the BIAS pin cannot be connected to VOUT.
Are there any concerns about shorting the BIAS pin to GND?
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460 , LM73606 Hi team,
My customer considers to use LM62460 as alternative option of LM73606 because of delivery issue.
Could you please pin pitch which is marked as red circle in below screenshot…