Part Number: LM62460 Hello, customer needs Iout=5A. Has the LM62460 and LM62495 same efficiency? And temperature behaviour is the same? What are the differences of LM62460 and LM62460-Q1?
Regards, Holger
Part Number: LM61495-Q1 Other Parts Discussed in Thread: LM61495 , LM62460 , LM61480 Hi I see in the datasheet that for the three part numbers: LM61495, LM61480, LM62460 they are rated for 6A,8A, and 10A, and are drop-in pin-compatible. However, I don't see…
Part Number: LM62460 Hi team,
Could you help to review my customer schematic of LM62460QRPHRQ1? if you can I will send the file to you in private, thanks.
Part Number: LM70840-Q1 Other Parts Discussed in Thread: LM62460-Q1 , LM61495-Q1 , LM61480-Q1 , LM62460 , LM70880-Q1 Tool/software: Hi, Team
I got three questions from customer regarding LM70840-Q1 functional Safety.
1. is this device satisfied with ISO26262…
Part Number: LM62460 Dear Specialists,
My customer is interested in LM62460 and would like to know when is the RTM.
Could you please let us know the current RTM schedule.
I appreciate your great help in advance.
Best regards,
Shinichi
Part Number: LM62460-Q1 Other Parts Discussed in Thread: LM62460
Hello
I need help with determining of phase margin. We need to use this buck converter at specific operation conditions: Vin=5.2,9,15,20 and Vout=5V/3A. Based on the PSPICE simulation, the…
Part Number: LM62460 Hi,
if I insert VUVLO=7V on with top resistor =100K the excel file return 15K, webech return 24K3. What is it the right value?
What is it the tollerance of Vuvlo with 1% resistor value?
Part Number: LM62460RPHEVM Other Parts Discussed in Thread: LM62460 Tool/software: Hi
I'm working with TIDA020047 board, but i need to power on my TIDA020047 with 24V instead of the recommanded input power 12V. so should I modify the refernce design…
Part Number: LM62460 Hi, I have three questions.
①I want to use LM62460 for Type-C.
When lowering the output voltage by changing the ratio of FB resistance,
the FB voltage rises and overvoltage protection works. Is this okay?
②The tss2 written in the…