Part Number: LM73100EVM Hi, I was wondering what were the layout recommendations regarding the LM73100RPWR chip and thermal vias for two devices in a Priority Power MUX Configuration, with one input 5VDC 1.2A, and the second battery backup, 3.2 VDC at 2.0A…
Part Number: LM73100EVM Hello TI experts,
My customer considers LM73100 for their new product, they just drew 1st schematic.
as same as the schematic, they will use 2 LM73100.
the point is, 2 outputs are tied together. and each output have a possibility…
Part Number: LM73100EVM
Hi
Use EVM of LM73100 to make Oring circuit, when one of them has no input,
The LM73100 without electricity has leakage at the DV/DT pin, which is about 16.xV When the input voltage is 19V
1. Will it cause damage to the IC? …
Part Number: LM73100EVM Hello expert,
Customer would like to know what is the condition to enter test mode. Since we mention pin 10 DNC is internal test pin and they are wondering if LM73100 has test mode. Thanks a lot!!
Best regards,
Ann Lien
Part Number: LM73100EVM Hi, I was wondering when you will have a pspice model available for the LM73100. Looking to use several of them for power path control and want to sim the switch over points.
Thanks.
Part Number: LM7310 Hi, LM73100 support team
In LM73100EVM schematic, a series resistor is added to a capacitor on dVdt pin. This series resistor is not considered in Design_Calculator. In this case, how to calculate the soft-start time?
Regards,
…
Other Parts Discussed in Thread: LM73100EVM , LM7310 Hello,
There is formula and example for R_IMON value calculation in the datasheet (SNOSDC0A – OCTOBER 2020 – REVISED DECEMBER 2020):
How it is possible to get 549ohm with that? I guess there…
Hi Premlatha,
I don't know whether your processor can handle 5V for 1us. But yes eFuse will take 1us to respond within which VOUT will follow VIN, I can only confirm this thing. Generally all our eFuse will have this much response time. If it is possible…