Part Number: LM76002-Q1 Other Parts Discussed in Thread: LM76002 , LM76002EVM-500K Hi all, I'm experiencing stability issues using the LM76002 buck regulator. Here's my schematic:
I'm using the TI LM76002EVM-500K dev kit, which I've modified to largely…
Part Number: LM76002-Q1 Tool/software: Thus far, looking at the data sheets I cannot see a difference beyond the labeling , although I wonder if the the difference may be in the manufacturing ie performance tested vs guaranteed by design. Are you able…
Part Number: LM76002 Tool/software: Hi expert,
My customer would like to know the open short test result and behaivor at specific pins as below. Do we have any data?
OPEN test
1. VCC w/o 2.2uF bypass capacitor
2. FB open with PVIN=60V
3…
Part Number: LM76002 Other Parts Discussed in Thread: LMR51635 ,
Tool/software:
Hi Team,
Need to make a BUCK power supply, input DC 18~60V, output 24V, current 0.8~1.5A Can LM76002 or LMR51635 be implemented? 1. What should be noted about loop compensation…
Part Number: LM76002 Tool/software: Hi,
my customer is facing some overvoltage at the output during the soft start over the set outputvoltage.
He is using the part with an efuse at the input to prevent reverse current. During soft start in case…
Part Number: LM76002-Q1 Other Parts Discussed in Thread: LM76002 Tool/software:
Hello TI Technical Team,
I am using the LM76002QRNPTQ1 IC to step down from 19.5V to 5V , but I am facing an issue: The output voltage only reaches around 2.5V to 3V …
Part Number: LM76002
Hello team,
Since customer is working with TUV on the system level SIL3 process, they need to know the failure mode behavior with LM76002 as below.
Whenever the feedback resistors of either RFBT or RFBB is left open after…
Part Number: LM76002 Hi team,
Regarding the LM76002, please confirm.
As for the input capacitor, it is recommended to install a 10uF to 22uF decoupling capacitor. The NOTE below mentions the need to consider DC-BIAS. After considering DC-BIAS, for…
Part Number: LM76002 There is an article of the SBVA025 to talk about the New thermal Metrics. It suggests to using new thermal metric, JB to calculate the junction temp of device.
However, in the Webench tool it still using old thermal parameter…
Part Number: LM76002-Q1 Other Parts Discussed in Thread: LM76002 Tool/software: I want to simulate a buck converter circuit using LM76002 IC. Kindly provide an LTspice netlist if possible for the same.