Part Number: LM9061 I have my LM9061 connected to a FET and powered by an external supply. When I pass a voltage of less than 5V through the FET, the LM9061 starts shutting off. I can trace this to the fact that the reference pin voltage is increasing…
Part Number: LM9061 Other Parts Discussed in Thread: TPS2595 , TPS25982 , LM5060 Hi,
In the datasheet there is no much information on output capacitors. As for input side it is mentioned that he VCC pin must be bypassed with a capacitor with a value of at…
Part Number: LM9061 Other Parts Discussed in Thread: TPS2595 , TPS25982 , TPS2663 Hi I am new to electronic design and I think I am missing something fundamental but... I intend to use LM9061 to limit max current through an electric motor (DC controled with…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM5069 , TPS24720 Hello Sir,
1.) I am using LM9061-Q1 high side gate driver in one of my applications. I have done a calculation for worst case scenario and I am switching a mosfet with this high…
Part Number: LM9061 Other Parts Discussed in Thread: LM5060-Q1 Hi,
LM9061 is designed to be controlled by 5V logic and our board has only 3V3, can you suggest a good alternative solution that can work at 3V3.
Thanks,
Jani
Part Number: LM9061 Other Parts Discussed in Thread: BQ77905 , , LM5060-Q1 , LM5060 Hi all,
my requirement is to use an OVP circuit, to prevent from the customer to insert the wrong charger.
I was planning to use the LM9061 together with a battery pack …
Part Number: LM9061 Hi Sir
I saw Vgs doesn't have type value in datasheet
May I know how to confirm the Vgs voltage
Due to the same schematic ,IPB240N03S4l have 13.5V Vgs ,but NVMFS5C604NL is 7V
Thanks
Part Number: CSD18542KTT Other Parts Discussed in Thread: CSD18540Q5B , CSD19505KTT , LM9061-Q1 Hello Team,A. We want to select an N channel based on the following specifications.
90A continuous current 200A pulse (100uS) 150A pulse (1mS) Low RDSon Low input…
Part Number: LM9061-Q1 Dear Sir:
We reference datasheet figure 22 of LM9061-Q1 to design below circuit, Then Vout only 7.5V~8V , It can't turn on the MOS completely , What's wrong for this design? Does TI have some suggest to us? Thanks?…