Hi Michael,
Sorry to bother you.
Just double confirm.
Does TI have similar LM95234 function and use thermistor, not transistor solution??
Thanks for your reply.
Hi Janarbek,
See Figure 22 in the datasheet:
1. The command register is which register address you want to read from or write to. For example if you want to read the manufacturer ID, you will need to read register address 0xFE.
2. Address byte…
Other Parts Discussed in Thread: LM95234 Hi,
I would like to use LM95234 as a quad temperature sensor.
I don't need any Critical temperature monitoring and I don't want to use TCRIT output pins function.
Do I need to pull-up these outputs or can…
Other Parts Discussed in Thread: LM95234 , LM93 Hi,
I'm searching LM95234 IBIS model.
I have checked zip file including all available IBIS models.
but I didn't find it.
Would you give me LM95234 IBIS model?
Best Regards,
Kato / Japan dist…
Hi Kato-san,
Slowing the clock shouldn't be a problem. I don't quite sure what you mean by setting hold time. As long as you don't capture the LM95234 SDA from 300ns to 1050ns after SCL falling edge, you should be ok.
Aaron
Other Parts Discussed in Thread: LM95234 I have a SMS7621-060 diode connected to the LM95234 on channel 2. I have a 2n3904 connected to channel 1. the chip set up is as fallows.
read speed = constant diode model = MMBT3904; enable all remote not local;…
Other Parts Discussed in Thread: LM95234 Hello,
Is there any documentation for the LM95234 EVM board? What kind of interface does the board provide to the D+/D- inputs to evaluate remote performance to diodes on another board? Does it have discrete…
Other Parts Discussed in Thread: LM95234 On the address select, how does that work with regard to the part? If I need say three of these and want to use all three addresses, do we just order different p/n or something ? Is there a – suffix or something…
Other Parts Discussed in Thread: LM95234 If I am only using the internal temp sensor on the LM95234, do I need to hook anything to the D- or D1 + through D4 + channels ? Should I just ground them?
Other Parts Discussed in Thread: LM95234 We are using the LM95234 and are seeing errors on reads of the Common Status Register over I2C. As a test case, we set up the Command Byte to be 0x02 and repeatedly read the Command Status Register. For successful…