Part Number: LM96000 Tool/software: Hi Teams,
There is a question about the LM96000 customer, it has 3 PWM outputs and 4 TACH inputs. Can it be understood as a maximum of 4 fans, with 2 fans sharing 1 PWM? Thank you.
Part Number: LM96000 Tool/software: Hi Teams,
The temperature range of TI's LM96000 model is 0 ℃ -125 ℃. If the board operates in a low temperature environment of -40 ℃ and then heats up to 0 ℃ or above, can it still work normally If not possible, we…
Hey Jin Lin,
I was searching and came across this thread. Wanted to let you know that we did release a drop in replacement for MAX31790. Please take a look at FAN31790 . Pin-to-pin, Bom-to-bom, and completely compatible with existing host side software…
Part Number: LM96000 Tool/software: Hi Team:
The 9600 I2C tHD:DAT SPEC has maximum:930ns
but the I2C standard is not limit the maximum
so if the tHD:DAT value over the 930ns,is there any concern for this?
Thanks.
Part Number: LM96000 Tool/software: Hi Team,
we found on the LM96000 that Tach2 is sending signal, but the fan speed is displayed as 0, as shown below.
is there any register will affect the display of this part?
Part Number: LM96000 Team,
I did not see information about the title in the DS, may anyone can provide it to customer?
Customer need this for the thermal modeling, thanks.
Jeremy.
Part Number: LM96000 Hi Sir,
1. 0x5C 0x5D 0x5E commanded 0xE2 2. 0x30 0x31 0x32 commanded 0x00 and 0xFF. No change in fan speed was seen.
Is there anything else to modify?
Part Number: LM96000 Just ask what the process is for setting up pwm The symptom is that pwm cannot write, and ff is currently read. Operation 40 Register bit 1 Set 0, 5c register set to manual mode. Write pwm, cannot write
Part Number: LM96000 Hi Expert,
Our issue is that LM96000 REG 0x62 bit 5~7 can't set PWM on/off individually. We set REG 0x64~0x66 Minimum PWM to 0x80 and REG 0x62 bit 5~7 to 0. When REG 0x62 bit 5 change to 1, PWM1 become REG 0x64 setting and PWM 2…