Part Number: LM96000 Dear team
Would you like to help recommend?
1. LM96000 is a hardware monitor to control fan speed, so as long as the parameters are set, there is no need to control the fan speed through software, right?
2. Dose TI have reference design…
Part Number: LM96000 Hi Experts,
Could you please advise what kind of remote diode can be used for LM96000 remote sense pin other than MMBT3904? What specs (e.g. Vbe_sat or ?) do we need to take into consideration for selecting a suitable diode for these…
Part Number: LM96000 Hi team
Customer wants to use spike smoothing function because of the following waveforms.
They set as the below.
register 0x62 setting value (Min/Off, Spike Smoothing)
Initial setting : 0xe8
Measurement setting value : 0x00
…
Part Number: LM96000 Team,
Sometimes we got LM96000 fan speed information affected by noise.
May I know if you can provide the layout guideline, especially for TACH signal, to prevent the noise of fan speed information.
Thank you.
Part Number: LM96000 Hi Team,
We are looking for a suitable solution to replace NCT7491RQR2G.
Seems LM96000 is very similar with this competitor, but customer ask for PECI3.0 interface support.
Please kindly suggest the replacement which has PECI3.0 interface…
hi Josh,
thanks, but question is still there: what high level and low level for IDS mean? Which one is the actual current on the diode?
Adding a separate temperature sensing harness and shielded connectords seems way too much effort for this purpose…
Part Number: LM96000 Dear E2E,
Our customer is asking the user guide or sample code to correct operate LM96000 to control Fan speed by writing command.
BR,
Jason
Part Number: LM96000 Dear Team,
Do we have a fan controller up to 7 ports?
Or I should contact another product line?
If you have a suitable road map please drop me a mail.
BR
Kevin