Part Number: LMG1025-Q1 I am working on LMG1025-Q1 which assigned with two packages which are DEE and DRV. pinning diagram shows DRV is wider but when looking at mechanical dimension both look same with smaller difference in land pattern
Could you please…
Part Number: LMG1025-Q1 Tool/software: Hello
I was wondering if you know about a space grade alternative to the LMG1025-Q1 that can be used for pulsing a laser.
Part Number: LMG1025-Q1 Tool/software: Hi All,
I have a question about LMG1025-Q1. Please see the following value.
IOH(Peak source current):7A(Typ) IOL(Peak sink current):5A(Typ) Would you kindly tell us maximum current values for IOH and IOL in…
Part Number: LMG1025-Q1 Tool/software: Hi TI team,
According to the EVK guide, I’m considering adding a 470nF feedthrough capacitor for C4.
Unfortunately, there is no capacitor available with the size and value matching the EVK requirements & AEC…
Part Number: LMG1025-Q1 Other Parts Discussed in Thread: LMG1020 Tool/software: Hello
We need Unencrypted Spice model for the Part LMG1025-Q1,Please help us on same
Part Number: LMG1025-Q1 Tool/software: Hello TI Team,
Is it possible to operate 2~3 LMG1025-Q1 in parallel to drive a single GaN FET?
The purpose is to increase the driving strength while maintaining minimal propagation delay, similar to the LMG1025…
Part Number: LMG1025-Q1 Other Parts Discussed in Thread: LMG1020 Hi Team,
Hope youre doing well!
What the max frequency can LMG1025-Q1 support? Is there any relevant tool that can provide calculations? Thanks!
Hey,
Thanks for reaching out to TI with your questions.
The LMG1025-Q1 is a low-side driver and therefore does not have a bootstrap diode. Are you referring to the LMG1205 that is a half-bridge GaN driver?
If you are referring to the LMG1205 half…
Part Number: LMG1025-Q1 Tool/software: Hi Team,
Hope you're doing well!
Can LMG1025-Q1 use with LVCMOS18 input?I saw the VIH min is 1.7V which is too close to 1.8V. Is there any suitable solution for 1.8V logic use case?
Thanks!