Part Number: LMG1205 Tool/software: Hello, I have a question about the LMG1205 .
In the datasheet, section 7.3.1 Input and Output states:
"If the input signal for either of the two channels, HI or LI, is not used, the control pin must be tied to…
Part Number: PMP31349 Other Parts Discussed in Thread: LM5148 , LM5148-Q1 , LMG1205 Hi team,
I am working on a new Buck converter design using GaN. I have drawn the schematic based on the PMP31349 reference guide , but I have the following questions…
Part Number: LMG1205 Tool/software: Hello,
Can the "LM5113QDPRRQ1" or "LMG1205YFXR" component be used to control a DC motor?
For this, I would drive an H-bridge (MOSFETs) with two LM5113QDPRRQ1 or " LMG1205YFXR" drivers (one driver each for a half…
Part Number: LMG1025-Q1 Other Parts Discussed in Thread: LMG1205
Hi,
LMG1025-Q1 has a large internal bootstrap diode voltage drop design( 0.53@1mA (T=25 ℃), this will prevent the bootstrap capacitor voltage from being charged too high (5V-0.53V=4…
Part Number: LMG1205 Other Parts Discussed in Thread: SN6501 Hello, I am using ltspice software to simulate LMG1205. The model was downloaded from the non encrypted model on the official website, but I found that there is an issue with multiple errors…
Part Number: LMG1205 Hello Texas Instruments team,
I would like to ask a question about the part LMG1205YFXR . We would like to solder it using a SN/PB solder paste but since its Lead finish/ Ball material is SNAGCU what you would recommend for better…
Part Number: LMG1205 Hello team - can you help with the question below? Thanks!
Can you tell me what SAC finish these are? Look like SAC105 but not sure.
LMG1205YFXT/R
Part Number: LMG1205 Other Parts Discussed in Thread: LMG1210 , LM5113-Q1 , LM5108 Tool/software: Hi team,
Recently my customer want to kick-off a totem-pole PFC project in air-con, and I want to promote the GaNFET half bridge driver to customer. So…
Part Number: LMG1205 Hi,
I want to use the LMG1205 to drive two EPC2016C transistors in a half-bridge configuration at 6.78 MHz, with a duty cycle of 50% and an input voltage of 48V.
From what I've seen, the LMG1205HBEVM evaluation board can drive…
Part Number: LMG1205 Other Parts Discussed in Thread: LMG1210 Team,
We had a discussion about the output voltage undershoot already: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1138025/lmg1205-voltage…