Part Number: LMG2610 Other Parts Discussed in Thread: UCC28782 In a newly developed system I am measuring a 700 to 1000ns delay from INL going high to SW driving. I am using with UCC28782. I've tried to check all lockout conditions. INH is not high. AUX…
Part Number: LMG2610 Hello TI Support,
Regarding LMG2610RRGR, a customer recently received parts from us that were marked with an "X" which they did their due diligence in asking TI E2E and confirming that the "X" parts are supposed to be pre-production…
Part Number: LMG2610 Tool/software: Hello TI experts,
A SPICE model is needed for circuit simulation using the LMG2610 ( LMG2610R044RKLR) . A complex device like this requires an accurate model for virtual testing, and a simple custom symbol will not…
Part Number: LMG2610 Other Parts Discussed in Thread: UCC25661 , , LMG2650 I am designing a high volume, off-line 240W USB-C charger and am looking to implement a multiphase flyback active clamp arrangement. I need a controller that can: be synchronised…
Part Number: LMG2610 Tool/software: The received LMG2610RRGR has the marking "XLMG2610".
The marking "XLMG2610" should be the #XLMG2610RRGT.
What is the difference in between the #LMG2610 & #XLMG2610?
Part Number: LMG2610 Tool/software: I'm reviewing a design based around LMG2610 and see that the bootstrap capacitor used is 220nF. The maximum frequency of this flyback based design is roughly 250kHz.
Am I correctly to believe that this is too large…
Part Number: UCC28780 Other Parts Discussed in Thread: UCC24612 , , LMG2610 Tool/software: Subject: Transformer Design Guidance for 60W Adapter using UCC28780, UCC24612, and LMG2610
Message:
Dear TI Support Team,
I am currently designing a 60W…
Part Number: LMG2610 Hello,
I would like to ask you a question about LMG2610. TI's GaN products use the Direct-drive method, and are supposed to perform normally-off operation in dMode without cascode. Does LMG2610 also use the Direct-drive method?…
Part Number: LMG2610 Other Parts Discussed in Thread: LMG3411R050 , LMG3411R070 Hi,
We need to design a Buck converter with the following specs:
Vin 400VDC
Vout adj. 250VDC to 350VDC
Iout 1.7A max@350VDC, less at lower voltages
Would you recommend…
Part Number: UCC28782 Other Parts Discussed in Thread: LMG2610 Hello,
I checked the calculation of Csw when using LMG2610 using an Excel calculation tool. In the figure below of "Begin Input Here", the settings are made for LMG2610, but are my settings…