Part Number: LMH0041 Hello,
we interesting to purchase this item LMH0041SQE/NOPB
but we would like to check with you first, if we can get EVB (Evaluation board)
Part Number: LMH0041 Hi, all.
I'd like to use the LMH0041 to deserialize an HD-SDI camera. Its LVDS output will be connected to an FPGA but it seems that its LVDS output interface is an 5-bits wide LVDS with 5 data lines. However, the FPGA expects a…
Part Number: LMH0041 Other Parts Discussed in Thread: LMH0344 , Hi, all.
I designed HD-SDI DES(Receiver) Board of 2 versions below as below.
But it does not all work well.
The FPGA(Zed Board) did not recognize the LVDS signal well.
I would like to know…
Other Parts Discussed in Thread: LMH0041 Dear all.
Our customer will use LMH0041 with cascade connection. Pls. see attached file.
4532.LMH0041.pdf
In this case, is there no problem of jitter? Is Gitta resolve by each block? Does only delay occur?
Regards…
Dear all.
Do you have IP of FPGA-attach.
"For more information please contact your local TI Sales Office/Distributor" written in the datasheet.
Regards, PAN-M
Other Parts Discussed in Thread: LMH0041 , LMH1983 Hello,
Our aim is to generate 3 frequencies synchronized with SDI video clock provided by a LMH0041.
The 3 frequencies are :
74.25MHz 27Mhz 12.288MHz
or
74.25MHz/1,001 27MHz 12.288Mhz
The…
Other Parts Discussed in Thread: LMH0041 Dear Representative!
How many logic lells do FPGA need to implement 4 HD (not Full HD) channels on one FPGA (Spartan3 or Cyclone-3) with LMH0041 deserializer?
How is it possible to get IP core for FPGA if we buy…
Hi Mark,
1). Jitter noted in the LMH0044 vs cable length is the total jitter or it is both low and high frequency.
2). LMH0041 reclocker loop bandwidth is in order of MHz(~1.5MHz at HD) and thus it attenuates the high frequency jitter above 1.5MHz at…
Hi Ken
As my understanding as below anf may need check with you.
For BT656, the 913A/914A are not suit and suggest use "LMH0040 or the CLC021", for a deserializer, look at the "LMH0041 or LMH0031".
and i right?
…
Hi John,
The LMH0040 and LMH0050 are serializers from LVDS inputs to a single high-speed output. The LMH0041 and LMH0051 are deserializers from a single high-speed input to LVDS outputs.
The big difference is the type of signaling used for the high…